Part Number: TMDX654IDKEVM
Tool/software: Linux
Hello,
I used the following command to stat the build for SDK as advised here: http://software-dl.ti.com/processor-sdk-linux/esd/docs/05_03_00_07/linux/Overview_Building_the_SDK.html#processor-sdk-build-reference
However, I am getting the following error:
| make[5]: Nothing to be done for 'first'. | make[5]: Leaving directory '/home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/tests/auto/widgets/widgets/qtoolbox' | cd qopenglwidget/ && ( test -e Makefile || /home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/git/tests/auto/widgets/widgets/qopenglwidget/qopenglwidget.pro -qtconf /home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/bin/qt.conf ) && make -f Makefile | make[5]: Entering directory '/home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/tests/auto/widgets/widgets/qtoolbutton' | make[5]: Nothing to be done for 'first'. | make[5]: Leaving directory '/home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/tests/auto/widgets/widgets/qtoolbutton' | make[5]: Entering directory '/home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/tests/auto/widgets/widgets/qopenglwidget' | make[5]: Nothing to be done for 'first'. | make[5]: Leaving directory '/home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/tests/auto/widgets/widgets/qopenglwidget' | make[4]: Leaving directory '/home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/tests/auto/widgets/widgets' | make[3]: Leaving directory '/home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/tests/auto/widgets' | make[2]: Leaving directory '/home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/tests/auto' | ERROR: oe_runmake failed | make[1]: Leaving directory '/home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/build/tests' | WARNING: exit code 1 from a shell command. | ERROR: Function failed: do_compile (log file is located at /home/prateek/tisdk/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/aarch64-linux/qtbase/5.9.7+gitAUTOINC+81b29a44d2-r0.arago13.tisdk5.4/temp/log.do_compile.6070) ERROR: Task (/home/prateek/tisdk/oe-layersetup/sources/meta-qt5/recipes-qt/qt5/qtbase_git.bb:do_compile) failed with exit code '1'
Please advise.
Thanks,
Prateek