This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DRA72XEVM: Video quality issue when using 4 channels input for H264 decode + display

Part Number: DRA72XEVM

Tool/software: Linux

Hi TI,

We are using PVSDK_03_04 SDK in DRA72XEVM board. The usecase being executed is NullSrc + Decode + Display

Below is the usecase diagram:

NullSource (A15) -> Decode -> VPE -> Merge -> Sync -> Alg_DmaSwMs -> Merge_1

DispDistSrc_weston -> Merge_1

Merge_1 -> Display

The video display is slow as we are using 4 channels as input. So to fix this reduced the number of buffers from 6 to 2 for nullSrc as below:

pPrm->channelParams[chId].numBuffers = 2;

Video performance is improved, but could see flickers oftenly every 8-10 seconds of video playback. And also if there is any object/person moving, the same is not been displayed properly, macroblocks seems to get distorted during reconstruction. FYI, the input is H.264 encoded video (VGA resolution, 4 channels so 4 x VGA @ 30fps). Is the IVA H264 decoder capable of decoding 4 VGA resolution encoded video @ 30fps? [Datasheet says decoder performance is 2x1080 @ 30fps)

We are using HDMI display displayType == CHAINS_DISPLAY_TYPE_HDMI_1080P(chains_common.c). However, final product will be HDMI VGA.
Hence after decoding we are scaling video from VGA to QVGA to fit 4 channels into Mosaic display. (Using VPE here to scale video)

Could you please provide inputs to resolve these issues??

Note:

Without Merge video us not played, hence Merge has to be present in usecase because Merge fwds single buffer corresponding to each CH ID

VPE is necessar in our usecase, because we need to scale video from VGA to QVGA resolution, as the output HDMI display unit is VGA size

Regards,
Sudhi

  • Hi Ti,

    Below is additional information for this video quality issue.

           decPrm->dpbBufSizeInFrames  = DEC_LINK_DPB_SIZE_IN_FRAMES_DEFAULT;

           decPrm->algCreateStatus     = DEC_LINK_ALG_CREATE_STATUS_CREATE;

           decPrm->decodeFrameType     = DEC_LINK_DECODE_ALL;

           decPrm->processCallLevel    = DEC_LINK_FRAMELEVELPROCESSCALL;

           decPrm->targetMaxWidth      = ENCDEC_MAX_FRAME_WIDTH;

           decPrm->targetMaxHeight     = ENCDEC_MAX_FRAME_HEIGHT;

           decPrm->numBufPerCh         = 6;

           decPrm->defaultDynamicParams.targetBitRate = 1*1000*1000;

           decPrm->defaultDynamicParams.targetFrameRate = 30;

           decPrm->fieldMergeDecodeEnable = FALSE;

            switch (pObj->codecType)

           {

     case '1': /* H264 */

                   decPrm->format = SYSTEM_IVIDEO_H264BP;

                   decPrm->profile = 0;;

                   decPrm->displayDelay = 0;

                   break;

           }

    I have attached the sample video for depicting the issue (Flicker and macrblock distortion)

              

  • Hi,

    Just for debugging purpose, can you remove the weston link.

    You can directly feed alg_dmaswms output to display and check.

    I hope nullSrc is reading all 4 channel then you do not need merge link.

    You can directly connect vpe with sync link.

    Please share the usecase log after pressing p after 1 min to check is there any frame drop.

    Please make sure your threshold for sync link is sufficient.

    Regards,

    Anuj

  • Hi Anuj,

    Thanks for the information.

    As suggested, have removed both the Weston and Merge links. [ nullSrc is reading all 4 channels hence it worked by removing Merge Link]

    We have  directly connect vpe with sync link.

    Threshold for Sync Link is set as below:

    (pObj->SyncPrm).syncThreshold = 10000/*SYNC_DROP_THRESHOLD_IN_MSEC*/;

    (pObj->SyncPrm).syncDelta = 1000;

    I have attached the Usecase log, which contains framework statistics (pressing p) in interval of 30 secs, 60 seconds, 90 seconds, etc.

    Could you also pls suggest an optimum values for syncThreshold  & syncDelta.

    Regards,

    Sudhi

    TI_NoWestonMerge_Log1.txt

  • Hi Anuj,

    Thanks for the information.

    As suggested, have removed both the Weston and Merge links. [ nullSrc is reading all 4 channels hence it worked by removing Merge Link]

    We have  directly connect vpe with sync link.

    Threshold for Sync Link is set as below:

    (pObj->SyncPrm).syncThreshold = 10000/*SYNC_DROP_THRESHOLD_IN_MSEC*/;

    (pObj->SyncPrm).syncDelta = 1000;

    I have attached the Usecase log, which contains framework statistics (pressing p) in interval of 30 secs, 60 seconds, 90 seconds, etc.

    Could you also pls suggest an optimum values for syncThreshold  & syncDelta.

    Regards,

    Sudhi

    3247.TI_NoWestonMerge_Log1.txt

  • Hi Anuj,

    Thanks for the information.

    As suggested, have removed both the Weston and Merge links. [ nullSrc is reading all 4 channels hence it worked by removing Merge Link]

    We have  directly connect vpe with sync link. Without Weston Flickering is not seen. But could you pls help to rectify flickering with Weston because we need Weston to have QT app running on top of video layer.

    As suggested by you, after removing Westin and Merge, the video quality is still not improved, distortions in the macroblock reconstruction is still seen.

    Threshold for Sync Link is set as below:

    (pObj->SyncPrm).syncThreshold = 10000/*SYNC_DROP_THRESHOLD_IN_MSEC*/;

    (pObj->SyncPrm).syncDelta = 1000;

    I have attached the Usecase log, which contains framework statistics (pressing p) in interval of 30 secs, 60 seconds, 90 seconds, etc.

    Could you also pls suggest an optimum values for syncThreshold  & syncDelta.

    Regards,

    Sudhi

    2330.TI_NoWestonMerge_Log1.txt

  • Hi,

    Delta should be same as frame interval and threshold should be twice of frame interval.

    Regards,
    Anuj
  • Hi,

    Its been long since any update on this thread,

    I hope the issue is resolved, if not then please reply below or create anew thread for different queries.

    Regards,

    Anuj