Hi,
RidgeRun is glad to release the Free SDK for Leopard Board.
The SDK has the following features:
* ARM toolchain: gcc 4.x
* U-boot 1.2.0 bootloader:
* Framebuffer support for splash screens.
* Console over serial and USB.
* DFU support.
* RidgeRun uboot installer to flash the images generated by the SDK (UBL, Uboot, kernel and file system).
* Linux LSP kernel 2.6.18 + Real Time patches + Leopard board support.
* Integration with some of TI's newest packages for the DaVinci platforms, including:
* DVSDK 2.00.00.22.
* XDCTools 3.10.03.
* DMAI 1.20.00.06.
Visit our blog in order to check out the features of the SDK and get the download link.
http://www.ridgerun.com/blog/
Regards,
Miguel Aguilar
RidgeRun Embedded Solutions