This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM335X: PM firmware request fails

Part Number: PROCESSOR-SDK-AM335X

Tool/software: Linux

I had my Linux-3,12 lLinux kernel zImage /device tree image for Beagle bone Black, but the original work on my ubuntu 12 and its Weatern Digital 2TB HDD was dead stopped spinning Ihad 2 of them dead, it's night mare, so be very care full with WDHDD, now I have to use SDD, I ave a fre 100 GB and use them for my new Ubuntu14, and I ran into problem they got filled up very quickly 100% used  in using Build root to build Root Filesystem and Linux PC got crashed I had to used another Linux PC to move empty SSD to get it back to work, so I had many front to fight at the same time, Linux kernelsource . So I lost all source code to recompile to remove this PM problem. Could I have any info where to get this source. I down load Linux SDK from TI, it's huge 1+TB, but I 'munable to find any appropriate defconfig something like beagle bone or  am335x or the like

I greatly appreciate your time and effort to help me out with this issue

Thnaks & Best Regards,

Duy-Ky Nuyen