Hi,
I have question about DM335 EMIF's width. There are three sentences:
1. Datasheet SPRS528B -
"3.12 Device Boot Modes.
The DM335 ARM can boot from either Async EMIF (AEMIF/OneNand) or from ARM ROM..."
2. Datasheet SPRS528B -
"5.7.1.2 OneNAND.
The OneNAND features supported are as follows.
...Only 16-bit data bus widths"
3. "Asynchronous External Memory Interface (EMIF)", SPRUFZ1 -
"2.6 Program Execution.
...When executing code from the EMIF, the bus width must be configured to be an 8-bit data bus."
Which of this sentences are wrong?