This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5718: TPS6590379 autostart on power up

Part Number: AM5718

Tool/software: Linux

Hi All,

TPSTPS6590379 + AM5718 auto start on power up

Correctly, I understand that in order to automatically start the processor, you need
1. connect GPIO_7 to the VRTC_OUT pin from the TPS6590379 chip itself
2. connect the RESET input through a 5 volt supervisor
3. pin boot1 connect to VRTC_OUT

Is this enough to start automatically after 5 volts?