This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NAND ECC 1/4 bit



Hello.

could you please clarify the following issue?

 

sprufg5(ARM Subsystem): 11.1.1 Features: Boot from NAND: states that DM365 does not support 1-bit ECC (which is used in SLC flash devices).

In our product, we would like to use K9F1208UOC(DevID: 0x76) or MT29F1G08AACWP:C(DevID: 0xF1).

sprufg5(ARM Subsystem): 11.2.1.2 NAND Device IDs Supported: states the Device IDs 0x76 & 0xF1 are supported.

In Appro DM365 IPNC, the NAND flash is K9F5608U0D - SLC with 1-bit ECC.

So it looks like RBL does support 1-bit ECC.

Could you confirm that please?

Thank you in advance.