Part Number: AM5728
HI,
I am trying to understand the memory architecture of AM5728, in my project I am able to use DSP1, DSP2 and ARM cores without issue, I have the following doubts.
1. Below is the portion of map file of DSP1.
******************************************************************************
TMS320C6x Linker Unix v8.2.2
******************************************************************************
>> Linked Wed May 22 19:10:58 2019
OUTPUT FILE NAME: <dra7-dsp1-fw.xe66>
ENTRY POINT SYMBOL: "ti_sysbios_family_c64p_Hwi0" address: 9503f400
MEMORY CONFIGURATION
name origin length used unused attr fill
---------------------- -------- --------- -------- -------- ---- --------
L2SRAM 00800000 00040000 0000ea60 000315a0 RW X
OCMC_RAM1 40300000 00080000 00000000 00080000 RW X
OCMC_RAM2 40400000 00100000 00000000 00100000 RW X
OCMC_RAM3 40500000 00100000 00000000 00100000 RW X
EXT_CODE 95000000 00100000 0003f420 000c0be0 RW X
EXT_DATA 95100000 00100000 000a4444 0005bbbc RW
EXT_HEAP 95200000 00300000 00000000 00300000 RW
TRACE_BUF 9f000000 00060000 00008004 00057ffc RW
EXC_DATA 9f060000 00010000 00000000 00010000 RW
PM_DATA 9f070000 00020000 00000000 00020000 RW X
Below ia the portion of map file for DSP2
******************************************************************************
TMS320C6x Linker Unix v8.2.2
******************************************************************************
>> Linked Wed May 22 22:08:44 2019
OUTPUT FILE NAME: <dra7-dsp2-fw.xe66>
ENTRY POINT SYMBOL: "ti_sysbios_family_c64p_Hwi0" address: 95043000
MEMORY CONFIGURATION
name origin length used unused attr fill
---------------------- -------- --------- -------- -------- ---- --------
L2SRAM 00800000 00040000 0002a76c 00015894 RW X
OCMC_RAM1 40300000 00080000 00000000 00080000 RW X
OCMC_RAM2 40400000 00100000 00000000 00100000 RW X
OCMC_RAM3 40500000 00100000 00000000 00100000 RW X
EXT_CODE 95000000 00100000 00042f60 000bd0a0 RW X
EXT_DATA 95100000 00900000 00305a1c 005fa5e4 RW
EXT_HEAP 95a00000 00400000 00000000 00400000 RW
TRACE_BUF 9f000000 00060000 00008004 00057ffc RW
EXC_DATA 9f060000 00010000 00000000 00010000 RW
PM_DATA 9f070000 00020000 00000000 00020000 RW X
If we observe the different sections such as "EXT_CODE","EXT_DATA" and other sections from above tables, DSP1 and DSP2 is using the same origin address. I observe both the cores are running independently without issue. How is actually the memory being manged?
From device tree we allocate different CMA base address for DSP1 and DSP2, from map file we see that both cores are using same address for different sections. In resource table of DSP1 we are using below macro
#define PHYS_MEM_IPC_VRING 0x99000000
and in resource table of DSP2 we are using below macro
#define PHYS_MEM_IPC_VRING 0x9F000000
Can someone please explain how exacly the memory is being organzed and utilized by different cores?
2. I need to understand what the below API is acually doing
status = Resource_physToVirt(cmem_address, (UInt32 *)&cmem_ptr);
Is this API converting Physical address to virtual address? In Resource table am I supposed to use the virtual address anywhere?
From following section of resource table "PHYS_CMEM_IOBUFS" is the physical address and "DSP_CMEM_IOBUFS" is the corresponding virtual address.
#define DSP_CMEM_IOBUFS 0x85000000
#define PHYS_CMEM_IOBUFS 0xA0000000
{
TYPE_DEVMEM,
DSP_CMEM_IOBUFS, PHYS_CMEM_IOBUFS,
DSP_CMEM_IOBUFS_SIZE, 0, 0, "DSP_CMEM_IOBUFS",
},
Can someone provide clearity on this?
Thanks,
Janardan