Part Number: AM3354
Tool/software: Linux
Hi all!
I'm working on a custom made AM3354 board quite similar to a Beaglebone and I have a very weird issue I can't figure out.
Sometimes, when booting, the UART console will become completely scrambled (see log attached). When that happens, the product will still boot (we can hear the sound playing at startup and GUI is running) but none of the UART will work properly (we're using ttyS0 1 and 2) and we can't connect through USB either.
We checked with an oscilloscope and it looks like when the console is scrambles the UART is transmitting at ~150kbps instead of the standard 115200 as if the clock had been reconfigured.
Other weird thing, is that when the issue happens, it's always when attaching mtd partitions (either after attaching mtd9 or mtd12) so it looks like it might come from the NAND driver, but I couldn't find anything that could cause that in it.
Last thing is when the product starts properly, then it works without issues even for days, so I don't think it's a clock drifting issue.
Any ideas what could cause that?
Thanks!
Antoine
PS: I've attached 3 logs: 2 with failure and 1 goood.
U-Boot 2017.01-00460-g147d7c34b8-dirty (May 21 2019 - 17:02:17 +0200)
CPU : AM335X-GP rev 2.1
DRAM: 256 MiB
NAND: 512 MiB
MMC: OMAP SD/MMC: 0
*** Warning - bad CRC, using default environment
Hit any key to stop autoboot: 0
Loading from nand0, offset 0x200000
Image Name: Linux-4.9.69
Created: 2019-05-14 10:41:58 UTC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 5112384 Bytes = 4.9 MiB
Load Address: 82000000
Entry Point: 82000000
NAND read: device 0 offset 0x80000, size 0x40000
262144 bytes read: OK
## Booting kernel from Legacy Image at 82000000 ...
Image Name: Linux-4.9.69
Created: 2019-05-14 10:41:58 UTC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 5112384 Bytes = 4.9 MiB
Load Address: 82000000
Entry Point: 82000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Kernel Image ... OK
Loading Device Tree to 8df14000, end 8df21176 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.9.69 (aferran@build) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11) ) #1 PREEMPT Tue May 14 10:41:52 UTC 2019
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt:Machine model:
[ 0.000000] cma: Reserved 24 MiB at 0x8e000000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon)
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 64452
[ 0.000000] Kernel command line: mtdparts=omap2-nand.0:128k(NAND.SPL),128k(NAND.SPL.backup1),128k(NAND.SPL.backup2),128k(NAND.SPL.backup3),256k(NAND.kernel-dtb),1m(NAND.u-boot),128k(NAND.u-boot-env),128k(NAND.u-boot-env.backup1),12m(NAND.kernel),110m(NAND.rootfs),12m(NAND.kernel2),110m(NAND.rootfs2),-(NAND.data) console=ttyS0,115200n8 ubi.mtd=NAND.rootfs,2048 ubi.mtd=NAND.data,2048 root=ubi0:rootfs rw rootfstype=ubifs rootwait=1
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 220096K/260096K available (7168K kernel code, 598K rwdata, 2352K rodata, 1024K init, 753K bss, 15424K reserved, 24576K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xd0000000 - 0xff800000 ( 760 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xcfe00000 ( 254 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0800000 (8160 kB)
[ 0.000000] .init : 0xc0b00000 - 0xc0c00000 (1024 kB)
[ 0.000000] .data : 0xc0c00000 - 0xc0c959ec ( 599 kB)
[ 0.000000] .bss : 0xc0c97000 - 0xc0d53548 ( 754 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000014] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000033] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000044] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000808] clocksource_probe: no matching clocksources found
[ 0.000993] Console: colour dummy device 80x30
[ 0.001035] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[ 0.088883] pid_max: default: 32768 minimum: 301
[ 0.089007] Security Framework initialized
[ 0.089019] Yama: becoming mindful.
[ 0.089055] AppArmor: AppArmor disabled by boot time parameter
[ 0.089216] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089228] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.090138] CPU: Testing write buffer coherency: ok
[ 0.090200] ftrace: allocating 23864 entries in 70 pages
[ 0.155445] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.160127] devtmpfs: initialized
[ 0.171809] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.172219] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.172244] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.174087] pinctrl core: initialized pinctrl subsystem
[ 0.175146] NET: Registered protocol family 16
[ 0.177330] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.193786] omap_hwmod: debugss: _wait_target_disable failed
[ 0.258873] cpuidle: using governor ladder
[ 0.288860] cpuidle: using governor menu
[ 0.295592] OMAP GPIO hardware version 0.1
[ 0.309842] omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/nandflash_pins_default, deferring probe
[ 0.312480] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.312738] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[ 0.312749] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[ 0.347821] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.350058] usbcore: registered new interface driver usbfs
[ 0.350130] usbcore: registered new interface driver hub
[ 0.350257] usbcore: registered new device driver usb
[ 0.350692] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[ 0.350748] omap_i2c 4802a000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c1_pins, deferring probe
[ 0.350859] pps_core: LinuxPPS API ver. 1 registered
[ 0.350867] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.351444] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.351913] Advanced Linux Sound Architecture Driver Initialized.
[ 0.352508] NetLabel: Initializing
[ 0.352522] NetLabel: domain hash size = 128
[ 0.352527] NetLabel: protocols = UNLABELED CIPSOv4
[ 0.352596] NetLabel: unlabeled traffic allowed by default
[ 0.352970] clocksource: Switched to clocksource timer1
[ 0.398992] VFS: Disk quotas dquot_6.6.0
[ 0.399088] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.410081] NET: Registered protocol family 2
[ 0.410841] TCP established hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.410872] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.410896] TCP: Hash tables configured (established 2048 bind 2048)
[ 0.410970] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.410986] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.411140] NET: Registered protocol family 1
[ 0.411839] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.413892] audit: initializing netlink subsys (disabled)
[ 0.413979] audit: type=2000 audit(0.380:1): initialized
[ 0.414965] workingset: timestamp_bits=14 max_order=16 bucket_order=2
[ 0.423289] zbud: loaded
[ 0.430647] NET: Registered protocol family 38
[ 0.430952] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 250)
[ 0.431146] io scheduler noop registered
[ 0.431159] io scheduler deadline registered
[ 0.431371] io scheduler cfq registered (default)
[ 0.432775] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.434533] Serial: 8250/16550 driver, 6 ports, IRQ sharing disabled
[ 0.437140] console [ttyS0] disabled
[ 0.437227] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a 8250
[ 1.078229] console [ttyS0] enabled
[ 1.082681] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 159, base_baud = 3000000) is a 8250
[ 1.092420] 48024000.serial: ttyS2 at MMIO 0x48024000 (irq = 160, base_baud = 3000000) is a 8250
[ 1.103114] SSFDC read-only Flash Translation layer
[ 1.108028] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.115040] PPP generic driver version 2.4.2
[ 1.120070] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.126712] ehci-platform: EHCI generic platform driver
[ 1.132119] ehci-omap: OMAP-EHCI Host Controller driver
[ 1.138632] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0
[ 1.145987] i2c /dev entries driver
[ 1.150681] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.158638] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.165858] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 1.171896] omap-aes 53500000.aes: will run requests pump with realtime priority
[ 1.180791] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 1.187952] hidraw: raw HID events driver (C) Jiri Kosina
[ 1.195372] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1.201437] NET: Registered protocol family 10
[ 1.207242] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 1.214879] NET: Registered protocol family 17
[ 1.219397] Key type dns_resolver registered
[ 1.223988] omap_voltage_late_init: Voltage driver support not added
[ 1.230746] ThumbEE CPU extension supported.
[ 1.235926] registered taskstats version 1
[ 1.240163] zswap: loaded using pool lzo/zbud
[ 1.246781] Key type encrypted registered
[ 1.255158] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 1.260348] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 1.268334] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xcc
[ 1.275002] nand: Micron MT29F4G16ABADAH4
[ 1.279035] nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
[ 1.286729] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme
[ 1.292119] 13 cmdlinepart partitions found on MTD device omap2-nand.0
[ 1.298725] Creating 13 MTD partitions on "omap2-nand.0":
[ 1.304191] 0x000000000000-0x000000020000 : "NAND.SPL"
[ 1.311041] 0x000000020000-0x000000040000 : "NAND.SPL.backup1"
[ 1.318443] 0x000000040000-0x000000060000 : "NAND.SPL.backup2"
[ 1.325788] 0x000000060000-0x000000080000 : "NAND.SPL.backup3"
[ 1.332938] 0x000000080000-0x0000000c0000 : "NAND.kernel-dtb"
[ 1.340225] 0x0000000c0000-0x0000001c0000 : "NAND.u-boot"
[ 1.347822] 0x0000001c0000-0x0000001e0000 : "NAND.u-boot-env"
[ 1.355057] 0x0000001e0000-0x000000200000 : "NAND.u-boot-env.backup1"
[ 1.362897] 0x000000200000-0x000000e00000 : "NAND.kernel"
[ 1.379592] 0x000000e00000-0x000007c00000 : "NAND.rootfs"
[ 1.476584] 0x000007c00000-0x000008800000 : "NAND.kernel2"
[ 1.493287] 0x000008800000-0x00000f600000 : "NAND.rootfs2"
[ 1.590350] 0x00000f600000-0x000020000000 : "NAND.data"
[ 1.848725] random: fast init done
[ 1.855956] input: tps65217_pwrbutton as /devices/platform/ocp/44e0b000.i2c/i2c-0/0-0024/tps65217-pwrbutton/input/input0
[ 1.867743] tps65217 0-0024: TPS65217 ID 0xe version 1.2
[ 2.195382] input: EP0110M09 as /devices/platform/ocp/44e0b000.i2c/i2c-0/0-0038/input/input1
[ 2.204852] at24 0-0050: 4096 byte 24c32 EEPROM, writable, 32 bytes/write
[ 2.211703] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 2.218470] i2c i2c-1: of_i2c: invalid reg on /ocp/i2c@4802a000/battery
[ 2.225192] i2c i2c-1: Failed to create I2C device for /ocp/i2c@4802a000/battery
[ 2.233085] bq27xxx-battery 1-0055: support ver. 1.2.0 enabled
[ 2.267346] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 400 kHz
[ 2.275322] ubi0: attaching mtd9
[ 2.662832] ubi0: scanning is finished
[ 2.681183] ubi0: volume 0 ("rootfs") re-sized from 763 to 796 LEBs
[ 2.688295] ubi0: attached mtd9 (name "NAND.rootfs", size 110 MiB)
[ 2.694573] ubi0: PEB size: 131072 bytes (128 KiB), LEB size: 126976 bytes
[ 2.701478] ubi0: min./max. I/O unit sizes: 2048/2048, sub-page size 512
[ 2.708225] ubi0: VID header offset: 2048 (aligned 2048), data offset: 4096
[ 2.715229] ubi0: good PEBs: 880, bad PEBs: 0, corrupted PEBs: 0
[ 2.721260] ubi0: user volume: 1, internal volumes: 1, max. volumes count: 128
[ 2.728527] ubi0: max/mean erase counter: 1/0, WL threshold: 4096, image sequence number: 1906782207
[ 2.737710] ubi0: available PEBs: 0, total reserved PEBs: 880, PEBs reserved for bad PEB handling: 80
[ 2.746992] ubi0: background thread "ubi_bgt0d" started, PID 98
[ 2.753011] ubi1: attaching mtd12
]@I▒iIl_▒e▒@Y&▒}U5!T▒sV]kR▒]@I▒mJ"d_▒eU@Q▒gT▒▒Z\▒@D{RaCV▒%c▒E@Yk@▒x@Q3F▒▒A@▒▒%M▒▒@S3M
▒▒&▒kMTlI▒h@6y▒▒eH1sQ▒S▒cݪ@I▒dK ▒]ֳ
▒]@I▒aJ▒l_▒e▒@W▒u]W-▒▒u!ZEy▒&▒kY▒aJׅaJ▒▒[▒▒cS▒c]▒dHl▒▒HPXLVlJ׃▒x@▒▒@▒iR▒mӦ▒5@`Li▒▒kR`JWeAR▒!WjwR@JVxG▒▒@▒▒-KV`_▒e▒V@Sui@▒&wMdH▒IQ▒K▒V@H1oY▒aZ▒▒Sd5@▒T_!@▒XLVdH▒▒▒▒x@^kY▒o▒▒kMTP@▒▒kYy@▒y[ݳ5@▒UQ▒iW▒SkYTs{W@I▒]@I▒iK▒d_▒#cH▒c\ukPEX\S!ѥm▒*5@▒@▒ZkY▒eiM▒`M▒@U]3k▒▒{Rk@▒{Q5@BlM▒`H▒T_!@▒XL)dJ׃▒▒x@▒cTU'iR
▒Y▒Y@ޥcVkYmR▒K▒F@H`FYPk▒mRXi@▒&!Ԕ%iT55@▒]@I▒mMWp_▒e▒@P\soٵmR▒q▒T!▒W_▒J3R▒yP▒kR▒SRTtG▒]@I▒qK▒p_TuaZ@SVu_іyW▒AHT▒!Gԧc▒*/XyӅk▒
sW▒▒Z▒mY\U▒{▒Umؖ%G▒HPXL▒`I▒▒▒▒_YV`JT▒HXXV▒@Y▒iT5!YWiR1yWf▒iW`HօeGV`H`LV▒ZDuJi`J▒DG▒]@I▒qJRd_▒SkцumT▒5@T▒cQUeoFу▒HPXL▒lIփ▒▒$▒IS▒gR▒EgZ▒T▒!@▒XL▒▒lKVmW▒%gP▒▒!ӥ}Re]@I▒eIl_▒�▒mPhH@PTsoٵ}R▒qXTC!AmY▒oZ▒äȖcX▒9@R$!H▒]@I▒mM▒l_▒▒▒▒mP▒`E▒iP▒!▒sW
▒X▒▒kRTqЦePw▒WU3g_e▒aU▒;▒^T]UwQ+▒T]Շ▒PwuGU▒]@K▒eIt_▒▒▒▒mPxH@R▒▒!YV7k@▒qZV▒%i▒▒]@K▒iM d_▒"SS▒mP▒`E$ET:b@ݵmڔ▒Pk▒U!H▒oV▒5!Hac▒%▒W▒mY▒T▒]@K▒mK▒▒@MY▒eT`EdKQTcݪ@I▒tK ▒]!▒`@%#F▒E}▒ec\GeV▒!▒kY▒aJ!s▒*?I▒`@6iR▒T_▒▒H▒XMVdHփ▒▒Ֆ!▒W!MV▒AR▒cݪ@M▒lJ▒`@&y▒▒uK▒TEF▒pK▒$EٕYWmP▒s]▒`H▒pL▒y▒▒q@Y)@)@V▒#F▒▒▒H▒XMVhHփ▒▒Ֆ!DS1MV▒AX\kY[i@▒u@▒▒yM@P▒kY▒AU▒]@K▒eKih_▒▒▒▒mPxH@W▒c@▒u֔5@K\X▒Qy▒U![֕1D▒[T
U-Boot 2017.01-00460-g147d7c34b8-dirty (May 21 2019 - 17:02:17 +0200)
CPU : AM335X-GP rev 2.1
Model:
DRAM: 256 MiB
Reset Source: Power-on reset has occurred.
NAND: 512 MiB
MMC: OMAP SD/MMC: 0
Hit any key to stop autoboot: 0
Loading from nand0, offset 0x200000
Image Name: Linux-4.9.69
Created: 2019-05-14 10:41:58 UTC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 5112384 Bytes = 4.9 MiB
Load Address: 82000000
Entry Point: 82000000
NAND read: device 0 offset 0x80000, size 0x40000
262144 bytes read: OK
## Booting kernel from Legacy Image at 82000000 ...
Image Name: Linux-4.9.69
Created: 2019-05-14 10:41:58 UTC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 5112384 Bytes = 4.9 MiB
Load Address: 82000000
Entry Point: 82000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Kernel Image ... OK
Loading Device Tree to 8df14000, end 8df21176 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.9.69 (aferran@build) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11) ) #1 PREEMPT Tue May 14 10:41:52 UTC 2019
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt:Machine model:
[ 0.000000] cma: Reserved 24 MiB at 0x8e000000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon)
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 64452
[ 0.000000] Kernel command line: mtdparts=omap2-nand.0:128k(NAND.SPL),128k(NAND.SPL.backup1),128k(NAND.SPL.backup2),128k(NAND.SPL.backup3),256k(NAND.kernel-dtb),1m(NAND.u-boot),128k(NAND.u-boot-env),128k(NAND.u-boot-env.backup1),12m(NAND.kernel),110m(NAND.rootfs),12m(NAND.kernel2),110m(NAND.rootfs2),-(NAND.data) console=ttyS0,115200n8 ubi.mtd=NAND.rootfs,2048 ubi.mtd=NAND.data,2048 root=ubi0:rootfs rw rootfstype=ubifs rootwait=1
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 220096K/260096K available (7168K kernel code, 598K rwdata, 2352K rodata, 1024K init, 753K bss, 15424K reserved, 24576K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xd0000000 - 0xff800000 ( 760 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xcfe00000 ( 254 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0800000 (8160 kB)
[ 0.000000] .init : 0xc0b00000 - 0xc0c00000 (1024 kB)
[ 0.000000] .data : 0xc0c00000 - 0xc0c959ec ( 599 kB)
[ 0.000000] .bss : 0xc0c97000 - 0xc0d53548 ( 754 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000015] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000032] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000043] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000801] clocksource_probe: no matching clocksources found
[ 0.000989] Console: colour dummy device 80x30
[ 0.001032] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[ 0.088896] pid_max: default: 32768 minimum: 301
[ 0.089020] Security Framework initialized
[ 0.089031] Yama: becoming mindful.
[ 0.089067] AppArmor: AppArmor disabled by boot time parameter
[ 0.089232] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089242] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.090159] CPU: Testing write buffer coherency: ok
[ 0.090223] ftrace: allocating 23864 entries in 70 pages
[ 0.155544] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.160236] devtmpfs: initialized
[ 0.171924] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.172330] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.172354] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.174210] pinctrl core: initialized pinctrl subsystem
[ 0.175271] NET: Registered protocol family 16
[ 0.177476] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.193940] omap_hwmod: debugss: _wait_target_disable failed
[ 0.258887] cpuidle: using governor ladder
[ 0.288872] cpuidle: using governor menu
[ 0.295574] OMAP GPIO hardware version 0.1
[ 0.309819] omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/nandflash_pins_default, deferring probe
[ 0.312452] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.312712] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[ 0.312723] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[ 0.347825] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.350074] usbcore: registered new interface driver usbfs
[ 0.350149] usbcore: registered new interface driver hub
[ 0.350275] usbcore: registered new device driver usb
[ 0.350710] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[ 0.350766] omap_i2c 4802a000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c1_pins, deferring probe
[ 0.350880] pps_core: LinuxPPS API ver. 1 registered
[ 0.350888] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.351462] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.351937] Advanced Linux Sound Architecture Driver Initialized.
[ 0.352534] NetLabel: Initializing
[ 0.352547] NetLabel: domain hash size = 128
[ 0.352553] NetLabel: protocols = UNLABELED CIPSOv4
[ 0.352621] NetLabel: unlabeled traffic allowed by default
[ 0.353000] clocksource: Switched to clocksource timer1
[ 0.399094] VFS: Disk quotas dquot_6.6.0
[ 0.399188] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.410178] NET: Registered protocol family 2
[ 0.410933] TCP established hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.410965] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.410989] TCP: Hash tables configured (established 2048 bind 2048)
[ 0.411064] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.411080] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.411243] NET: Registered protocol family 1
[ 0.411944] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.413994] audit: initializing netlink subsys (disabled)
[ 0.414080] audit: type=2000 audit(0.380:1): initialized
[ 0.415069] workingset: timestamp_bits=14 max_order=16 bucket_order=2
[ 0.423406] zbud: loaded
[ 0.430779] NET: Registered protocol family 38
[ 0.431084] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 250)
[ 0.431288] io scheduler noop registered
[ 0.431299] io scheduler deadline registered
[ 0.431509] io scheduler cfq registered (default)
[ 0.432913] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.434672] Serial: 8250/16550 driver, 6 ports, IRQ sharing disabled
[ 0.437287] console [ttyS0] disabled
[ 0.437374] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a 8250
[ 1.078375] console [ttyS0] enabled
[ 1.082848] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 159, base_baud = 3000000) is a 8250
[ 1.092597] 48024000.serial: ttyS2 at MMIO 0x48024000 (irq = 160, base_baud = 3000000) is a 8250
[ 1.103316] SSFDC read-only Flash Translation layer
[ 1.108229] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.115271] PPP generic driver version 2.4.2
[ 1.120304] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.126947] ehci-platform: EHCI generic platform driver
[ 1.132357] ehci-omap: OMAP-EHCI Host Controller driver
[ 1.138855] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0
[ 1.146215] i2c /dev entries driver
[ 1.150932] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.158905] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.166117] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 1.172159] omap-aes 53500000.aes: will run requests pump with realtime priority
[ 1.181055] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 1.188226] hidraw: raw HID events driver (C) Jiri Kosina
[ 1.195659] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1.201736] NET: Registered protocol family 10
[ 1.207541] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 1.215168] NET: Registered protocol family 17
[ 1.219690] Key type dns_resolver registered
[ 1.224285] omap_voltage_late_init: Voltage driver support not added
[ 1.231054] ThumbEE CPU extension supported.
[ 1.236227] registered taskstats version 1
[ 1.240464] zswap: loaded using pool lzo/zbud
[ 1.247088] Key type encrypted registered
[ 1.255462] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 1.260651] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 1.268656] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xcc
[ 1.275338] nand: Micron MT29F4G16ABADAH4
[ 1.279370] nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
[ 1.287062] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme
[ 1.292452] 13 cmdlinepart partitions found on MTD device omap2-nand.0
[ 1.299060] Creating 13 MTD partitions on "omap2-nand.0":
[ 1.304525] 0x000000000000-0x000000020000 : "NAND.SPL"
[ 1.311370] 0x000000020000-0x000000040000 : "NAND.SPL.backup1"
[ 1.318784] 0x000000040000-0x000000060000 : "NAND.SPL.backup2"
[ 1.326134] 0x000000060000-0x000000080000 : "NAND.SPL.backup3"
[ 1.333376] 0x000000080000-0x0000000c0000 : "NAND.kernel-dtb"
[ 1.340577] 0x0000000c0000-0x0000001c0000 : "NAND.u-boot"
[ 1.348192] 0x0000001c0000-0x0000001e0000 : "NAND.u-boot-env"
[ 1.355416] 0x0000001e0000-0x000000200000 : "NAND.u-boot-env.backup1"
[ 1.363325] 0x000000200000-0x000000e00000 : "NAND.kernel"
[ 1.379966] 0x000000e00000-0x000007c00000 : "NAND.rootfs"
[ 1.476959] 0x000007c00000-0x000008800000 : "NAND.kernel2"
[ 1.493657] 0x000008800000-0x00000f600000 : "NAND.rootfs2"
[ 1.590736] 0x00000f600000-0x000020000000 : "NAND.data"
[ 1.848757] random: fast init done
[ 1.855792] input: tps65217_pwrbutton as /devices/platform/ocp/44e0b000.i2c/i2c-0/0-0024/tps65217-pwrbutton/input/input0
[ 1.867598] tps65217 0-0024: TPS65217 ID 0xe version 1.2
[ 2.195412] input: EP0110M09 as /devices/platform/ocp/44e0b000.i2c/i2c-0/0-0038/input/input1
[ 2.204870] at24 0-0050: 4096 byte 24c32 EEPROM, writable, 32 bytes/write
[ 2.211721] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 2.218476] i2c i2c-1: of_i2c: invalid reg on /ocp/i2c@4802a000/battery
[ 2.225197] i2c i2c-1: Failed to create I2C device for /ocp/i2c@4802a000/battery
[ 2.233083] bq27xxx-battery 1-0055: support ver. 1.2.0 enabled
[ 2.267359] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 400 kHz
[ 2.275369] ubi0: attaching mtd9
]@H▒qI▒p_▒e\V@Y&▒mT5!▒▒c▒UaR▒D▒]@H▒uHyp_▒e\V@Q▒cQ▒'!VK3H▒kRTeCW▒▒oWkwA▒s▒▒dH▒DE▒T▒]@H▒uKYt_▒eT@X▒U▒▒I2`K▒s▒:!▒Vp@%3F▒$E▒&▒kMhJ▒h@6yҶT[!@▒XKtL▒▒▒x@Uu-▒qGt@▒Ey▒&▒kY▒!JוaJ▒m[▒▒c▒
▒U▒▒)I▒T_▒PXKdL׃▒x@▒▒@▒iZ▒mۦ▒5@`Li▒▒kR`JWeAR▒c▒5m▒J5@ dJ▒▒@´%IVd_▒eTV@Sui@▒wMpH%cRV@H1oY▒q▒J!▒▒5@▒T[!@▒XKhJփ▒h@VkY▒o▒▒kMP@▒▒kYiH▒i▒%wMP@U▒-H▒i▒%w▒▒mZ▒!L▒▒@´!I▒p_▒eTV@W/▒Tg!R6▒k▒▒}▒*5@▒@▒ZkY▒eiM▒`M▒@UU7kȦ▒{Zk@▒k▒*5▒`J▒hH▒▒UAH▒mHWl_▒e\V@Q
c▒TgkH▒wMP@ޥcVTk▒*}Z
▒St5@`F
▒YPk▒}R
▒W▒c5ei֕55@▒]@H▒mL▒h_▒eTV@PTwoٵmZ▒a▒iH▒eԃ▒▒AY^▒yR▒@X▒tL▒U@H▒aH▒p_▒e▒V@Q▒cYuoȥiH▒T▒]@I▒iH)`_▒e▒V@Y&▒m\5!▒▒c▒UaR▒"]
U-Boot 2017.01-00460-g147d7c34b8-dirty (May 21 2019 - 17:02:17 +0200) CPU : AM335X-GP rev 2.1 Model: DRAM: 256 MiB Reset Source: Power-on reset has occurred. NAND: 512 MiB MMC: OMAP SD/MMC: 0 Hit any key to stop autoboot: 0 Loading from nand0, offset 0x200000 Image Name: Linux-4.9.69 Created: 2019-05-14 10:41:58 UTC Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 5112384 Bytes = 4.9 MiB Load Address: 82000000 Entry Point: 82000000 NAND read: device 0 offset 0x80000, size 0x40000 262144 bytes read: OK ## Booting kernel from Legacy Image at 82000000 ... Image Name: Linux-4.9.69 Created: 2019-05-14 10:41:58 UTC Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 5112384 Bytes = 4.9 MiB Load Address: 82000000 Entry Point: 82000000 Verifying Checksum ... OK ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Kernel Image ... OK Loading Device Tree to 8df14000, end 8df21176 ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.9.69 (aferran@build) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11) ) #1 PREEMPT Tue May 14 10:41:52 UTC 2019 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt:Machine model: [ 0.000000] cma: Reserved 24 MiB at 0x8e000000 [ 0.000000] Memory policy: Data cache writeback [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.1 (sgx neon) [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 64452 [ 0.000000] Kernel command line: mtdparts=omap2-nand.0:128k(NAND.SPL),128k(NAND.SPL.backup1),128k(NAND.SPL.backup2),128k(NAND.SPL.backup3),256k(NAND.kernel-dtb),1m(NAND.u-boot),128k(NAND.u-boot-env),128k(NAND.u-boot-env.backup1),12m(NAND.kernel),110m(NAND.rootfs),12m(NAND.kernel2),110m(NAND.rootfs2),-(NAND.data) console=ttyS0,115200n8 ubi.mtd=NAND.rootfs,2048 ubi.mtd=NAND.data,2048 root=ubi0:rootfs rw rootfstype=ubifs rootwait=1 [ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes) [ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) [ 0.000000] Memory: 220096K/260096K available (7168K kernel code, 598K rwdata, 2352K rodata, 1024K init, 753K bss, 15424K reserved, 24576K cma-reserved, 0K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB) [ 0.000000] vmalloc : 0xd0000000 - 0xff800000 ( 760 MB) [ 0.000000] lowmem : 0xc0000000 - 0xcfe00000 ( 254 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0xc0008000 - 0xc0800000 (8160 kB) [ 0.000000] .init : 0xc0b00000 - 0xc0c00000 (1024 kB) [ 0.000000] .data : 0xc0c00000 - 0xc0c959ec ( 599 kB) [ 0.000000] .bss : 0xc0c97000 - 0xc0d53548 ( 754 kB) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 [ 0.000000] Preemptible hierarchical RCU implementation. [ 0.000000] Build-time adjustment of leaf fanout to 32. [ 0.000000] NR_IRQS:16 nr_irqs:16 16 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz [ 0.000014] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns [ 0.000031] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns [ 0.000042] OMAP clocksource: timer1 at 24000000 Hz [ 0.000807] clocksource_probe: no matching clocksources found [ 0.000995] Console: colour dummy device 80x30 [ 0.001037] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736) [ 0.088900] pid_max: default: 32768 minimum: 301 [ 0.089026] Security Framework initialized [ 0.089038] Yama: becoming mindful. [ 0.089074] AppArmor: AppArmor disabled by boot time parameter [ 0.089239] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.089250] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.090156] CPU: Testing write buffer coherency: ok [ 0.090220] ftrace: allocating 23864 entries in 70 pages [ 0.155477] Setting up static identity map for 0x80100000 - 0x80100060 [ 0.160148] devtmpfs: initialized [ 0.171834] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 0.172244] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.172268] futex hash table entries: 256 (order: -1, 3072 bytes) [ 0.174123] pinctrl core: initialized pinctrl subsystem [ 0.175182] NET: Registered protocol family 16 [ 0.177371] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.193817] omap_hwmod: debugss: _wait_target_disable failed [ 0.258888] cpuidle: using governor ladder [ 0.288879] cpuidle: using governor menu [ 0.295591] OMAP GPIO hardware version 0.1 [ 0.309828] omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/nandflash_pins_default, deferring probe [ 0.312476] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.312724] omap4_sram_init:Unable to allocate sram needed to handle errata I688 [ 0.312735] omap4_sram_init:Unable to get sram pool needed to handle errata I688 [ 0.347819] edma 49000000.edma: TI EDMA DMA engine driver [ 0.350054] usbcore: registered new interface driver usbfs [ 0.350129] usbcore: registered new interface driver hub [ 0.350254] usbcore: registered new device driver usb [ 0.350694] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe [ 0.350749] omap_i2c 4802a000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c1_pins, deferring probe [ 0.350860] pps_core: LinuxPPS API ver. 1 registered [ 0.350868] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.351444] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400 [ 0.351912] Advanced Linux Sound Architecture Driver Initialized. [ 0.352503] NetLabel: Initializing [ 0.352517] NetLabel: domain hash size = 128 [ 0.352522] NetLabel: protocols = UNLABELED CIPSOv4 [ 0.352591] NetLabel: unlabeled traffic allowed by default [ 0.352961] clocksource: Switched to clocksource timer1 [ 0.398937] VFS: Disk quotas dquot_6.6.0 [ 0.399032] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.410000] NET: Registered protocol family 2 [ 0.410750] TCP established hash table entries: 2048 (order: 1, 8192 bytes) [ 0.410780] TCP bind hash table entries: 2048 (order: 1, 8192 bytes) [ 0.410804] TCP: Hash tables configured (established 2048 bind 2048) [ 0.410879] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.410895] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.411045] NET: Registered protocol family 1 [ 0.411752] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available [ 0.413803] audit: initializing netlink subsys (disabled) [ 0.413889] audit: type=2000 audit(0.380:1): initialized [ 0.414887] workingset: timestamp_bits=14 max_order=16 bucket_order=2 [ 0.423207] zbud: loaded [ 0.430559] NET: Registered protocol family 38 [ 0.430863] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 250) [ 0.431067] io scheduler noop registered [ 0.431080] io scheduler deadline registered [ 0.431291] io scheduler cfq registered (default) [ 0.432689] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568 [ 0.434467] Serial: 8250/16550 driver, 6 ports, IRQ sharing disabled [ 0.437084] console [ttyS0] disabled [ 0.437170] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a 8250 [ 1.078183] console [ttyS0] enabled [ 1.082626] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 159, base_baud = 3000000) is a 8250 [ 1.092377] 48024000.serial: ttyS2 at MMIO 0x48024000 (irq = 160, base_baud = 3000000) is a 8250 [ 1.102938] SSFDC read-only Flash Translation layer [ 1.107987] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.114990] PPP generic driver version 2.4.2 [ 1.120010] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 1.126654] ehci-platform: EHCI generic platform driver [ 1.132063] ehci-omap: OMAP-EHCI Host Controller driver [ 1.138555] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0 [ 1.145908] i2c /dev entries driver [ 1.150639] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 1.158607] cpuidle: enable-method property 'ti,am3352' found operations [ 1.165828] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2 [ 1.171866] omap-aes 53500000.aes: will run requests pump with realtime priority [ 1.180758] omap-sham 53100000.sham: hw accel on OMAP rev 4.3 [ 1.187919] hidraw: raw HID events driver (C) Jiri Kosina [ 1.195330] ip_tables: (C) 2000-2006 Netfilter Core Team [ 1.201404] NET: Registered protocol family 10 [ 1.207217] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 1.214846] NET: Registered protocol family 17 [ 1.219364] Key type dns_resolver registered [ 1.223955] omap_voltage_late_init: Voltage driver support not added [ 1.230711] ThumbEE CPU extension supported. [ 1.235885] registered taskstats version 1 [ 1.240123] zswap: loaded using pool lzo/zbud [ 1.246759] Key type encrypted registered [ 1.255137] omap-gpmc 50000000.gpmc: GPMC revision 6.0 [ 1.260324] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000 [ 1.268308] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xcc [ 1.274981] nand: Micron MT29F4G16ABADAH4 [ 1.279013] nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64 [ 1.286704] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme [ 1.292094] 13 cmdlinepart partitions found on MTD device omap2-nand.0 [ 1.298704] Creating 13 MTD partitions on "omap2-nand.0": [ 1.304170] 0x000000000000-0x000000020000 : "NAND.SPL" [ 1.311012] 0x000000020000-0x000000040000 : "NAND.SPL.backup1" [ 1.318419] 0x000000040000-0x000000060000 : "NAND.SPL.backup2" [ 1.325761] 0x000000060000-0x000000080000 : "NAND.SPL.backup3" [ 1.332919] 0x000000080000-0x0000000c0000 : "NAND.kernel-dtb" [ 1.340193] 0x0000000c0000-0x0000001c0000 : "NAND.u-boot" [ 1.347804] 0x0000001c0000-0x0000001e0000 : "NAND.u-boot-env" [ 1.355018] 0x0000001e0000-0x000000200000 : "NAND.u-boot-env.backup1" [ 1.362862] 0x000000200000-0x000000e00000 : "NAND.kernel" [ 1.379551] 0x000000e00000-0x000007c00000 : "NAND.rootfs" [ 1.476539] 0x000007c00000-0x000008800000 : "NAND.kernel2" [ 1.493221] 0x000008800000-0x00000f600000 : "NAND.rootfs2" [ 1.590281] 0x00000f600000-0x000020000000 : "NAND.data" [ 1.848715] random: fast init done [ 1.855738] input: tps65217_pwrbutton as /devices/platform/ocp/44e0b000.i2c/i2c-0/0-0024/tps65217-pwrbutton/input/input0 [ 1.867536] tps65217 0-0024: TPS65217 ID 0xe version 1.2 [ 2.195368] input: EP0110M09 as /devices/platform/ocp/44e0b000.i2c/i2c-0/0-0038/input/input1 [ 2.204832] at24 0-0050: 4096 byte 24c32 EEPROM, writable, 32 bytes/write [ 2.211683] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 2.218436] i2c i2c-1: of_i2c: invalid reg on /ocp/i2c@4802a000/battery [ 2.225164] i2c i2c-1: Failed to create I2C device for /ocp/i2c@4802a000/battery [ 2.233053] bq27xxx-battery 1-0055: support ver. 1.2.0 enabled [ 2.267339] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 400 kHz [ 2.275308] ubi0: attaching mtd9 [ 2.683384] ubi0: scanning is finished [ 2.693620] ubi0: attached mtd9 (name "NAND.rootfs", size 110 MiB) [ 2.699842] ubi0: PEB size: 131072 bytes (128 KiB), LEB size: 126976 bytes [ 2.706807] ubi0: min./max. I/O unit sizes: 2048/2048, sub-page size 512 [ 2.713555] ubi0: VID header offset: 2048 (aligned 2048), data offset: 4096 [ 2.720545] ubi0: good PEBs: 880, bad PEBs: 0, corrupted PEBs: 0 [ 2.726589] ubi0: user volume: 1, internal volumes: 1, max. volumes count: 128 [ 2.733856] ubi0: max/mean erase counter: 2/0, WL threshold: 4096, image sequence number: 1906782207 [ 2.743040] ubi0: available PEBs: 0, total reserved PEBs: 880, PEBs reserved for bad PEB handling: 80 [ 2.752309] ubi0: background thread "ubi_bgt0d" started, PID 98 [ 2.758299] ubi1: attaching mtd12 [ 3.745957] ubi1: scanning is finished [ 3.757694] ubi1: attached mtd12 (name "NAND.data", size 266 MiB) [ 3.763927] ubi1: PEB size: 131072 bytes (128 KiB), LEB size: 126976 bytes [ 3.770832] ubi1: min./max. I/O unit sizes: 2048/2048, sub-page size 512 [ 3.777580] ubi1: VID header offset: 2048 (aligned 2048), data offset: 4096 [ 3.784585] ubi1: good PEBs: 2128, bad PEBs: 0, corrupted PEBs: 0 [ 3.790703] ubi1: user volume: 1, internal volumes: 1, max. volumes count: 128 [ 3.797970] ubi1: max/mean erase counter: 2/1, WL threshold: 4096, image sequence number: 223907004 [ 3.807066] ubi1: available PEBs: 0, total reserved PEBs: 2128, PEBs reserved for bad PEB handling: 80 [ 3.816438] ubi1: background thread "ubi_bgt1d" started, PID 99 [ 3.823353] input: gpio_buttons@0 as /devices/platform/gpio_buttons@0/input/input2 [ 3.831456] omap_rtc 44e3e000.rtc: setting system clock to 2000-01-01 00:00:02 UTC (946684802) [ 3.840643] vmmcsd_fixed: disabling [ 3.844220] ALSA device list: [ 3.847200] No soundcards found. [ 3.863006] UBIFS (ubi0:0): background thread "ubifs_bgt0_0" started, PID 100 [ 3.882487] UBIFS (ubi0:0): recovery needed [ 3.935115] UBIFS (ubi0:0): recovery completed [ 3.939717] UBIFS (ubi0:0): UBIFS: mounted UBI device 0, volume 0, name "rootfs" [ 3.947187] UBIFS (ubi0:0): LEB size: 126976 bytes (124 KiB), min./max. I/O unit sizes: 2048 bytes/2048 bytes [ 3.957163] UBIFS (ubi0:0): FS size: 99676160 bytes (95 MiB, 785 LEBs), journal size 9023488 bytes (8 MiB, 72 LEBs) [ 3.967656] UBIFS (ubi0:0): reserved for root: 0 bytes (0 KiB) [ 3.973530] UBIFS (ubi0:0): media format: w4/r0 (latest is w4/r0), UUID 6434B2D7-7480-4C7D-B611-53ADA68805BD, small LPT model [ 3.985614] VFS: Mounted root (ubifs filesystem) on device 0:14. [ 3.992860] devtmpfs: mounted [ 3.997149] Freeing unused kernel memory: 1024K INIT: version 2.88 booting [ 4.363181] UBIFS (ubi1:1): background thread "ubifs_bgt1_1" started, PID 115 [ 4.389988] UBIFS (ubi1:1): recovery needed [ 4.457858] UBIFS (ubi1:1): recovery completed [ 4.462463] UBIFS (ubi1:1): UBIFS: mounted UBI device 1, volume 1, name "data" [ 4.469764] UBIFS (ubi1:1): LEB size: 126976 bytes (124 KiB), min./max. I/O unit sizes: 2048 bytes/2048 bytes [ 4.479741] UBIFS (ubi1:1): FS size: 258142208 bytes (246 MiB, 2033 LEBs), journal size 9023488 bytes (8 MiB, 72 LEBs) [ 4.490498] UBIFS (ubi1:1): reserved for root: 0 bytes (0 KiB) [ 4.496372] UBIFS (ubi1:1): media format: w4/r0 (latest is w4/r0), UUID 592578A4-4B1A-45C5-A0C8-96F874E8193F, small LPT model INIT: Entering runlevel: 3 Starting logging: OK Populating /dev using udev: [ 4.957744] udevd[141]: starting version 3.2.5 [ 5.024534] udevd[142]: starting eudev-3.2.5 [ 5.364084] 47401300.usb-phy supply vcc not found, using dummy regulator [ 5.387276] rtc-pcf85263 0-0051: rtc core: registered rtc-pcf85263 as rtc1 [ 5.453248] rtc-pcf85263 0-0051: PCF85263 RTC (irqpin=INTA irq=27) [ 5.549781] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20 [ 5.798247] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle [ 5.810760] remoteproc remoteproc0: wkup_m3 is available [ 5.815345] davinci_evm sound: tlv320aic3x-hifi <-> 4803c000.mcasp mapping ok [ 5.889525] PM: Cannot get wkup_m3_ipc handle [ 5.894366] remoteproc remoteproc0: powering up wkup_m3 [ 5.909351] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 220832 [ 5.909620] remoteproc remoteproc0: remote processor wkup_m3 is now up [ 5.909649] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x193 [ 6.039803] PM: bootloader does not support rtc-only! [ 6.140434] fbtft: module is from the staging directory, the quality is unknown, you have been warned. [ 6.155318] fb_st7789v: module is from the staging directory, the quality is unknown, you have been warned. [ 6.167372] fbtft_of_value: width = 240 [ 6.171242] fbtft_of_value: height = 240 [ 6.175798] fbtft_of_value: buswidth = 8 [ 6.179770] fbtft_of_value: debug = 0 [ 6.183850] fbtft_of_value: rotate = 180 [ 6.187795] fbtft_of_value: fps = 50 [ 6.500923] graphics fb0: fb_st7789v frame buffer, 240x240, 112 KiB video memory, 4 KiB DMA buffer memory, fps=50, spi1.0 at 24 MHz done Initializing random number generator... done. Starting system message bus: done Starting network: OK Starting ip over usb: [ 6.984320] using random self ethernet address [ 6.988812] using random host ethernet address [ 6.997818] usb0: HOST MAC 16:aa:c2:28:59:6e [ 7.004284] usb0: MAC 0e:53:c4:2e:ec:78 [ 7.008211] using random self ethernet address [ 7.012674] using random host ethernet address [ 7.017835] g_ether gadget: Ethernet Gadget, version: Memorial Day 2008 [ 7.024772] g_ether gadget: g_ether ready [ 7.044884] IPv6: ADDRCONF(NETDEV_UP): usb0: link is not ready login: