Other Parts Discussed in Thread: TMS320DM6437
Hi,
Well I'm currently writing a module to display a rectangle on a RGB Image (bmp file).
I'm using TMS320DM6437 & Code Composer Studio-CSS 3.3v for Coding.
Within BSP(provided for TMS320DM6437 ) there is a function which draws Rectangle i.e. GRAPHICS_DrawRectangle.
void GRAPHICS_DrawRect(volatile u16* pDstBuf, volatile Uint16 x1, volatile Uint16 y1, volatile Uint16 x2, volatile Uint16 y2, volatile Uint16 color, volatile Bool fill, volatile u8 bufindex);
I can draw the rectangle only on binary images (bmp file) properly, but i'm facing problem to draw it on RGB image.
Image size is - 640 x 480
pls guide suggesting any alterative / sloution to draw rectangle on RGB Image.
Presently code is in simulation mode only.
Regards,
Pratibha