Hello,
I have a video file that has been run through the ArcSoft Mediaconverter tool to convert it to a format compatible with the DM355. I extracted the mpeg4 elemental stream using ffmpeg. I can look at the elemental video (with a m4v extension) using VLC on the PC and playback is fine. I change the extension to .mpeg4 and play it back using the decode demo. Frustratingly, I wind up with some strange green noise coming up in waves from the bottom of the screen. See the attached pics. The green IS dependent on what is happening in the video. If the video is moving down, off the bottom of the screen, no noise appears. If the video is moving UP towards the top of the screen, this green nonsense gets dragged into the picture. Plus there are a few lines of white noise at the bottom that are not seen in the original or viewing with VLC.
Any ideas?