Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: TPS65910
Tool/software: TI-RTOS
Hi,
I am new to am335x device, I want boot the board from memory card, but it is not booting from mmc instead of it is booing from nand always,
here is the u-boot o/p for mmc dev 1
=======================================
PRCHECK# mmc dev 1
data abort
pc : [<9ff5ff00>] lr : [<9ff5f101>]
reloc pc : [<8081ef00>] lr : [<8081e101>]
sp : 9ef16cd0 ip : 9ff46cdd fp : 00000003
r10: 9ffb2f4c r9 : 9ef20ed8 r8 : 9ef27e28
r7 : 9ff46865 r6 : 9ef27568 r5 : 9ef275e0 r4 : 47810000
r3 : 9ff5fef1 r2 : 0002340f r1 : 9ffa3dea r0 : 9ef275e0
Flags: nZCv IRQs off FIQs on Mode SVC_32
Resetting CPU ...
resetting ...
U-Boot SPL 2016.05-00304-gad06f64-dirty (Jul 05 2018 - 09:51:03)
###TPS65910##
Trying to boot from NAND
The Expected Linux image was not found. Please check your NAND configuration.
Trying to start u-boot now...
U-Boot 2016.05-00304-gad06f64-dirty (Aug 13 2018 - 19:21:18 +0530)
CPU : AM335X-GP rev 2.1
Model: TI AM335x EVM
Watchdog enabled
DRAM: 512 MiB
NAND: 512 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Card did not respond to voltage select!
** Bad device mmc 0 **
Using default environment
<ethaddr> not set. Validating first E-fuse MAC
Net: cpsw, usb_ether
Press SPACE to abort autoboot in 2 seconds
PRCHECK#
=======================================
please help me on this issue !!!