Part Number: AM3352
Other Parts Discussed in Thread: TPS65217, TCA8418
Tool/software: Linux
root@beaglebone:~#
root@beaglebone:~#
root@beaglebone:~#
root@beaglebone:~# startx
hostname: beaglebone: Unknown host
xauth: file /home/root/.serverauth.904 does not exist
xauth: file /home/root/.Xauthority does not exist
xauth: file /home/root/.Xauthority does not exist
X.Org X Server 1.16.3
Release Date: 2014-12-20
X Protocol Version 11, Revision 0
Build Operating System: Linux 4.4.0-143-generic x86_64
Current Operating System: Linux beaglebone 4.1.18-g6b41ca0b94 #3 SMP Tue May 28 00:12:04 IST 2019 armv7l
Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext4 rootwait fixrtc fixrtc coherent_pool=10M
Build Date: 23 February 2019 02:52:29PM
Current version of pixman: 0.32.6
Before reporting problems, check http://wiki.x.org
to make sure that you have the latest version.
Markers: (--) probed, (**) from config file, (==) default setting,
(++) from command line, (!!) notice, (II) informational,
(WW) warning, (EE) error, (NI) not implemented, (??) unknown.
(==) Log file: "/var/log/Xorg.1.log", Time: Mon May 27 18:47:03 2019
(==) Using system config directory "/usr/share/X11/xorg.conf.d"
/etc/X11/xinit/xinitrc: line 51: twm: command not found
/etc/X11/xinit/xinitrc: line 52: xclock: command not found
/etc/X11/xinit/xinitrc: line 55: exec: xterm: not found
/etc/X11/xinit/xinitrc: line 53: xterm: command not found
xinit: connection to X server lost
waiting for X server to shut down (EE) Server terminated successfully (0). Closing log file.
root@beaglebone:~#