This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DVSDK 3.10 and linux 2.6.32-rc2-davinci : umount locks at key removal

Hi,

I am trying to migrate our dm355 product from linux 2.6.18 to the dvsdk 3.10 (linux 2.6.32)  and I am facing some problems with the usb drive unmount.

Let me explain :

-I plug the key, the key is correctly recognized.

- I mount the key in /mnt/key for example

- I unplug the key without umounting it.

- I try to unmount the key but umount freezes and after 120 seconds i get  a "umount blocked for more than 120 seconds" message

I didn't change any linux configuration option concerning usb and we are using busybox 1.17.4. (I found on the busybox forum that it should be a kernel problem)

I found on internet that this is a known regression from linux kernel 2.6.31, but it seems reported at rc4 :

http://lkml.indiana.edu/hypermail/linux/kernel/0910.3/00585.html

It appears to be solved after rc7:

https://bugzilla.kernel.org/show_bug.cgi?id=14481

 

Does anyone as tried that on a DM355EVM ?

Did I do something wrong ?