Part Number: OMAP-L138
Other Parts Discussed in Thread: OMAP-L132
Hi
Just some short questions about the RTC of the OMAP-L138:
* The datasheet claims: "The RTC has a power supply that is isolated from the rest of the system." So what exactly does the SPLITPOWER bit do? Make it even more isolated ... ?
* The datasheet also claims: "If these power supplies are not isolated (CTRL.SPLITPOWER=0), RTC_CVDD must be equal to or greater than CVDD." As far as I understand the SPLITPOWER bit defaults to 0 and must be set by software. But what if my hardware gives RTC_CVDD to be LOWER than CVDD? How would I configure for that without powering the system?
* What happens when RTC_CVDD is lower then CVDD with SPLITPOWER=0 ? Could this damage the device? What would be the effect on the RTC or the CPU?
Thanks.