Part Number: TMS320DM368
Hi,
we have an existing product (not new design) on which we're trying to add a new video feature.
We want to achieve 1080p - 60fps
We are driving the TMS320DM368's VPBE with and external clock of 74.25 MHz.
With the current settings of our PLL we achieve 30 fps.
To get to 60 we have two options:
1) change the PLL settings doubling the internal frequency (keeping the external oscillator at 74.25 MHz)
2) doubling the external frequency and bringing that at 148.5 MHz
I don't think that the option 2) is viable.
The app note http://www.ti.com.cn/cn/lit/ug/sprufg9c/sprufg9c.pdf at pag. 59 sets the range of the external clock to 75 MHz.
Am I correct?
Thanks,
Alessandro