Part Number: TDA3LA
If I have a usecase as below:
UseCase: chains_radarMetawaveMonopulse
IssCapture -> Alg_RadarProcess_fft (DSP1) -> Dup_fft (DSP1)
Dup_fft (DSP1) -> Merge_swms (DSP1)
Dup_fft (DSP1) -> Alg_RadarProcess_pkDetect (DSP1) -> Merge_swms (DSP1)
Dup_fft (DSP1) -> Alg_RadarProcess_pkDetect (DSP1) -> Merge_swms (DSP1)
Merge_swms -> Alg_RadarProcess_guardRemoval (DSP1) -> Sync_network -> NetworkTx (IPU1_1)
The output of 2D FFT will produce 4 RDMs from 4 RX and 1 TX channels. It is then duplicated into 3 streams with 2 streams going into 2 pkDetect as inputs. We would like the two pkDetect links to operate on different RX channels. For example, we would like pkDetect 1 to process RX0 and RX1 while pkDetect 2 to process RX2 and RX3.
My question is how can we instruct (configure) each of the pkDetect link in the graph to process different RX channels. If both paths process all 4 RXes, that would be easy but we like them to only process 2 out of 4.
Thanks,
--Khai