Tool/software: Linux
Refer to the following links:
software-dl.ti.com/.../Overview_Building_the_SDK.html
I encountered the following problems when compiling SDK05.03.00.07 with Yocto:
| DEBUG: Executing shell function do_install
| cp: cannot stat '/home/adv/yocto_bsp/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ti-cgt-pru-native/2.2.1-r0/ti-cgt-pru-2.2.1_2.2.1/.': No such file or directory
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_install (log file is located at /home/adv/yocto_bsp/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/ti-cgt-pru-native/2.2.1-r0/temp/log.do_install.29364)