This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5718: Hardware design queries

Part Number: AM5718
Other Parts Discussed in Thread: AM5706, AM5708

Hi,

I want to use this AM5718AABCX Sitara based processor in my next project.

I have few queries regarding the H/W Design on Ethernet.

In my project I need to have 2 Ethernet Interface. As I can see from the Description It supports only one Ethernet Interface. But when I read the Ethernet Section It says GMAC_SW can be used as GMII and MII.

So it's indicating 2 Ethernet interface is possible. Am i right ?

If it supports only Single Ethernet Interface i'm planning to use External Ethernet  controller and communicating with the processor via serial interfaces like i2c/SPI. For eg., - KSZ8851SNL/SNLI from the Microchip which has PHY and MAC inside.

But I'm concerned about the speed.

And I really want to know How Ethernet Controller (MAC) will be communicating with processor (Inbuilt Ethernet).