This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TDA2SX: Linux halted when root from emmc

Part Number: TDA2SX

Tool/software: Linux

Hello,

I want to use the Linux to my own board card, which is started by emmc,and the processor is TDA2SX

Due to different hardware, I have modified the DTS file, attached is the DTS file I modified, and the log.txt file is the printed debugging information of kernel startup, which shows that emmc cannot be mounted.

dts.tar

buaawkp@buaawkp-computer:~$ sudo minicom 
[sudo] buaawkp 的密码: 


Welcome to minicom 2.7

OPTIONS: I18n 
Compiled on Nov 15 2018, 20:18:47.
Port /dev/ttyUSB0, 16:44:58

Press CTRL-A Z for help on special keys











































U-Boot SPL 2016.05-00013-g3331a8a-dirty (Jun 03 2019 - 11:42:05)
DRA752-GP ES2.0
no pinctrl for hs200_1_8v
no pinctrl for ddr_1_8v
Trying to boot from MMC2_2
reading dra7-ipu2-fw.lzop
spl_load_file_fat: error reading file dra7-ipu2-fw.lzop, err - -1
spl: error reading image dra7-ipu2-fw.lzop, err - -1
Error loading remotecore IPU2!,Continuing with boot ...
reading dra7-dsp1-fw.lzop
spl_load_file_fat: error reading file dra7-dsp1-fw.lzop, err - -1
spl: error reading image dra7-dsp1-fw.lzop, err - -1
Error loading remotecore DSP1!,Continuing with boot ...
reading dra7-dsp2-fw.lzop
spl_load_file_fat: error reading file dra7-dsp2-fw.lzop, err - -1
spl: error reading image dra7-dsp2-fw.lzop, err - -1
Error loading remotecore DSP2!,Continuing with boot ...
reading dra7-ipu1-fw.lzop
spl_load_file_fat: error reading file dra7-ipu1-fw.lzop, err - -1
spl: error reading image dra7-ipu1-fw.lzop, err - -1
Error loading remotecore IPU1!,Continuing with boot ...
spl: falcon_args_file not set in environment, falling back to default
reading single-stage-boot.dtb
spl_load_image_fat_os: error reading image single-stage-boot.dtb, err - -1
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img


U-Boot 2016.05-00013-g3331a8a-dirty (Jun 03 2019 - 11:42:05 +0800)

CPU  : DRA752-GP ES2.0
Model: TI DRA742
Board: DRA74x EVM REV 
DRAM:  1.5 GiB
MMC:   i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
OMAP SD/MMC: 0, OMAP SD/MMC: 1
Warning: fastboot.board_rev: unknown board revision
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid GPT ***
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid Backup GPT ***
ERROR: cannot find partition: 'userdata'

at arch/arm/cpu/armv7/omap-common/utils.c:199/mmc_get_part_size()
Warning: fastboot.userdata_size: unable to calc
SCSI:  SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst 
scanning bus for devices...
Found 0 device(s).
Net:   Could not get PHY for ethernet@48484000: addr 2
eth0: ethernet@48484000
Hit any key to stop autoboot:  0 
## Error: "board_findfdt" not defined
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
134 bytes read in 2 ms (65.4 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
3476592 bytes read in 28 ms (118.4 MiB/s)
107051 bytes read in 11 ms (9.3 MiB/s)
Booting from mmc1 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x350c70 ]
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   Loading Device Tree to 8ffe2000, end 8ffff22a ... OK
Using machid 0xfe6 from environment

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Initializing cgroup subsys cpuset
[    0.000000] Initializing cgroup subsys cpu
[    0.000000] Initializing cgroup subsys cpuacct
[    0.000000] Linux version 4.4.84-00039-g845ce97-dirty (wang@buaawkp) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #1 SMP PREEMPT 9
[    0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[    0.000000] Machine model: TI DRA742
[    0.000000] Reserved memory: created DMA memory pool at 0x0000000040300000, size 3 MiB
[    0.000000] Reserved memory: initialized node cmem@40300000, compatible id shared-dma-pool
[    0.000000] Reserved memory: regions without no-map are not yet supported
[    0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 80 MiB
[    0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created CMA memory pool at 0x000000009e000000, size 32 MiB
[    0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: regions without no-map are not yet supported
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000a1000000, size 32 MiB
[    0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000a3000000, size 32 MiB
[    0.000000] Reserved memory: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: regions without no-map are not yet supported
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a9000000, size 32 MiB
[    0.000000] Reserved memory: initialized node cmem@A9000000, compatible id shared-dma-pool
[    0.000000] cma: Reserved 24 MiB at 0x00000000be400000
[    0.000000] Forcing write-allocate cache policy for SMP
[    0.000000] Memory policy: Data cache writealloc
[    0.000000] OMAP4: Map 0x00000000bfd00000 to fe600000 for dram barrier
[    0.000000] DRA752 ES2.0
[    0.000000] PERCPU: Embedded 11 pages/cpu @ef62a000 s14912 r8192 d21952 u45056
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 251456
[    0.000000] Kernel command line: console=ttyO0,115200n8 vram=16M root=/dev/mmcblk1p2 ip=none mem=1024M cm6
[    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Memory: 394396K/1012736K available (6479K kernel code, 309K rwdata, 2312K rodata, 340K init, 288K bss, 413540K reserved, 204800)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
[    0.000000]     vmalloc : 0xf0800000 - 0xff800000   ( 240 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xf0000000   ( 768 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc089e04c   (8793 kB)
[    0.000000]       .init : 0xc089f000 - 0xc08f4000   ( 340 kB)
[    0.000000]       .data : 0xc08f4000 - 0xc0941420   ( 310 kB)
[    0.000000]        .bss : 0xc0943000 - 0xc098b000   ( 288 kB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000]  Build-time adjustment of leaf fanout to 32.
[    0.000000] NR_IRQS:16 nr_irqs:16 16
[    0.000000] ti_dt_clocks_register: failed to lookup clock node gmac_gmii_ref_clk_div
[    0.000000] OMAP clockevent source: timer1 at 32786 Hz
[    0.000000] Architected cp15 timer(s) running at 6.14MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[    0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[    0.000016] Switching to timer-based delay loop, resolution 162ns
[    0.000335] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[    0.000342] OMAP clocksource: 32k_counter at 32768 Hz
[    0.000784] Console: colour dummy device 80x30
[    0.000799] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[    0.000805] This ensures that you still see kernel messages. Please
[    0.000810] update your kernel commandline.
[    0.000823] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[    0.000836] pid_max: default: 32768 minimum: 301
[    0.000931] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.000941] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.001481] Initializing cgroup subsys io
[    0.001497] Initializing cgroup subsys memory
[    0.001521] Initializing cgroup subsys devices
[    0.001533] Initializing cgroup subsys freezer
[    0.001544] Initializing cgroup subsys perf_event
[    0.001555] Initializing cgroup subsys pids
[    0.001581] CPU: Testing write buffer coherency: ok
[    0.001780] /cpus/cpu@0 missing clock-frequency property
[    0.001796] /cpus/cpu@1 missing clock-frequency property
[    0.001805] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.001844] Setting up static identity map for 0x80008380 - 0x800083e0
[    0.080065] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[    0.080134] Brought up 2 CPUs
[    0.080147] SMP: Total of 2 processors activated (24.59 BogoMIPS).
[    0.080153] CPU: All CPU(s) started in HYP mode.
[    0.080158] CPU: Virtualization extensions available.
[    0.080532] devtmpfs: initialized
[    0.109324] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[    0.110292] omap_hwmod: l3_main_2 using broken dt data from ocp
[    0.312602] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[    0.312623] futex hash table entries: 512 (order: 3, 32768 bytes)
[    0.316848] pinctrl core: initialized pinctrl subsystem
[    0.317707] NET: Registered protocol family 16
[    0.318623] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.340221] cpuidle: using governor ladder
[    0.370241] cpuidle: using governor menu
[    0.378798] OMAP GPIO hardware version 0.1
[    0.385259] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 !
[    0.401903] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[    0.401916] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[    0.409801] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[    0.409810] hw-breakpoint: maximum watchpoint size is 8 bytes.
[    0.410214] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[    0.410223] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[    0.410822] OMAP DMA hardware revision 0.0
[    0.451551] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[    0.452694] edma 43300000.edma: memcpy is disabled
[    0.457534] edma 43300000.edma: TI EDMA DMA engine driver
[    0.461916] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[    0.462092] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[    0.462249] omap-iommu 58882000.mmu: 58882000.mmu registered
[    0.462407] omap-iommu 55082000.mmu: 55082000.mmu registered
[    0.462692] omap-iommu 41501000.mmu: 41501000.mmu registered
[    0.462875] omap-iommu 41502000.mmu: 41502000.mmu registered
[    0.466194] palmas 0-0058: IRQ missing: skipping irq request
[    0.481301] palmas: probe of 0-0058 failed with error -121
[    0.481563] pcf857x: probe of 0-0020 failed with error -121
[    0.481811] pcf857x: probe of 0-0021 failed with error -121
[    0.481969] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[    0.482371] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
[    0.482557] media: Linux media interface: v0.10
[    0.482613] Linux video capture interface: v2.00
[    0.482653] pps_core: LinuxPPS API ver. 1 registered
[    0.482660] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.482683] PTP clock support registered
[    0.482729] EDAC MC: Ver: 3.0.0
[    0.483487] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[    0.483787] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[    0.484862] clocksource: Switched to clocksource arch_sys_counter
[    0.495292] NET: Registered protocol family 2
[    0.495779] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[    0.495843] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[    0.495968] TCP: Hash tables configured (established 8192 bind 8192)
[    0.496017] UDP hash table entries: 512 (order: 2, 16384 bytes)
[    0.496047] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[    0.496250] NET: Registered protocol family 1
[    0.496506] RPC: Registered named UNIX socket transport module.
[    0.496515] RPC: Registered udp transport module.
[    0.496521] RPC: Registered tcp transport module.
[    0.496527] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.497489] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[    0.507632] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.508291] NFS: Registering the id_resolver key type
[    0.508316] Key type id_resolver registered
[    0.508323] Key type id_legacy registered
[    0.508400] ntfs: driver 2.1.32 [Flags: R/O].
[    0.509667] bounce: pool size: 64 pages
[    0.509812] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[    0.509827] io scheduler noop registered
[    0.509838] io scheduler deadline registered
[    0.509869] io scheduler cfq registered (default)
[    0.514263] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
[    0.517484] PCI host bridge /ocp/axi@0/pcie_rc@51000000 ranges:
[    0.517496]   No bus range found for /ocp/axi@0/pcie_rc@51000000, using [bus 00-ff]
[    0.517528]    IO 0x20003000..0x20012fff -> 0x00000000
[    0.517549]   MEM 0x20013000..0x2fffffff -> 0x20013000
[    0.547604] dra7-pcie 51000000.pcie_rc: link is not up
[    0.547779] dra7-pcie 51000000.pcie_rc: PCI host bridge to bus 0000:00
[    0.547791] pci_bus 0000:00: root bus resource [bus 00-ff]
[    0.547801] pci_bus 0000:00: root bus resource [io  0x0000-0xffff]
[    0.547811] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[    0.548214] PCI: bus0: Fast back to back transfers disabled
[    0.548332] PCI: bus1: Fast back to back transfers enabled
[    0.548414] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[    0.548429] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[    0.548441] pci 0000:00:00.0: PCI bridge to [bus 01]
[    0.548658] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
[    0.609398] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[    0.612748] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 301, base_baud = 3000000) is a 8250
[    1.619101] console [ttyS0] enabled
[    1.623494] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 302, base_baud = 3000000) is a 8250
[    1.633197] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 303, base_baud = 3000000) is a 8250
[    1.643208] [drm] Initialized drm 1.1.0 20060810
[    1.648754] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    1.655440] [drm] No driver support for vblank timestamp query.
[    1.661572] [drm] Initialized vdrm 1.0.0 20110917 on minor 0
[    1.674335] loop: module loaded
[    1.677860] vmemexp device MAJOR num = 245
[    1.681987] vmemexp class registered
[    1.685722] /dev/vmemexp device registered
[    1.689836] ioctl DBUFIOC_EXPORT_VIRTMEM = -1072899120
[    1.695529] nand: No NAND device found
[    1.699301] omap2-nand 8000000.nand: scan failed, may be bus-width mismatch
[    1.709289] m25p80 spi32766.0: found s25fl512s, expected s25fl256s1
[    1.978543] m25p80 spi32766.0: s25fl512s (65536 Kbytes)
[    1.983849] 7 ofpart partitions found on MTD device spi32766.0
[    1.989728] Creating 7 MTD partitions on "spi32766.0":
[    1.994906] 0x000000000000-0x000000040000 : "QSPI.SPL"
[    2.001042] 0x000000040000-0x000000140000 : "QSPI.u-boot"
[    2.007416] 0x000000140000-0x0000001c0000 : "QSPI.u-boot-spl-os"
[    2.014358] 0x0000001c0000-0x0000001d0000 : "QSPI.u-boot-env"
[    2.020152] mtd: partition "QSPI.u-boot-env" doesn't end on an erase block -- force read-only
[    2.029643] 0x0000001d0000-0x0000001e0000 : "QSPI.u-boot-env.backup1"
[    2.036200] mtd: partition "QSPI.u-boot-env.backup1" doesn't start on an erase block boundary -- force read-only
[    2.057404] 0x0000001e0000-0x0000009e0000 : "QSPI.kernel"
[    2.062826] mtd: partition "QSPI.kernel" doesn't start on an erase block boundary -- force read-only
[    2.082944] 0x0000009e0000-0x000002000000 : "QSPI.file-system"
[    2.088822] mtd: partition "QSPI.file-system" doesn't start on an erase block boundary -- force read-only
[    2.100828] libphy: Fixed MDIO Bus: probed
[    2.154893] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
[    2.161019] davinci_mdio 48485000.mdio: detected phy mask fffffffe
[    2.169186] libphy: 48485000.mdio: probed
[    2.173219] davinci_mdio 48485000.mdio: phy[0]: device 48485000.mdio:00, driver unknown
[    2.181940] cpsw 48484000.ethernet: Detected MACID = 6c:c3:74:33:3c:6a
[    2.188631] cpsw 48484000.ethernet: cpts: overflow check period 800
[    2.195653] cpsw 48484000.ethernet: cpsw: Detected MACID = 6c:c3:74:33:3c:6b
[    2.204262] mousedev: PS/2 mouse device common for all mice
[    2.210457] i2c /dev entries driver
[    2.219809] omap_hsmmc 4809c000.mmc: Got CD GPIO
[    2.225468] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[    2.231853] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[    2.358842] ledtrig-cpu: registered to indicate activity on CPUs
[    2.366926] NET: Registered protocol family 10
[    2.372371] sit: IPv6 over IPv4 tunneling driver
[    2.378634] NET: Registered protocol family 17
[    2.383308] Key type dns_resolver registered
[    2.387713] omap_voltage_late_init: Voltage driver support not added
[    2.394615] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[    2.400845] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[    2.407095] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
[    2.413685] Power Management for TI OMAP4+ devices.
[    2.418815] Registering SWP/SWPB emulation handler
[    2.425039] dmm 4e000000.dmm: workaround for errata i878 in use
[    2.432609] dmm 4e000000.dmm: initialized all PAT entries
[    2.439075] [drm] Initialized omapdrm 1.0.0 20110917 on minor 1
[    2.446748] omap_hsmmc 4809c000.mmc: Got CD GPIO
[    2.452504] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[    2.458957] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[    2.465954] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[    2.472164] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[    2.478454] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
[    2.485476] hctosys: unable to open rtc device (rtc0)
[    2.502450] evm_1v8: disabling
[    2.505556] evm_3v3_sw: disabling
[    2.508887] aic_dvdd: disabling
[    2.512039] vmmcwl_fixed: disabling
[    2.515561] pbias_mmc_omap5: disabling
[    2.520529] VFS: Cannot open root device "mmcblk1p2" or unknown-block(0,0): error -6
[    2.528366] Please append a correct "root=" boot option; here are the available partitions:
[    2.536784] 1f00             256 mtdblock0  (driver?)
[    2.541870] 1f01            1024 mtdblock1  (driver?)
[    2.546979] 1f02             512 mtdblock2  (driver?)
[    2.552062] 1f03              64 mtdblock3  (driver?)
[    2.557166] 1f04              64 mtdblock4  (driver?)
[    2.562249] 1f05            8192 mtdblock5  (driver?)
[    2.567354] 1f06           22656 mtdblock6  (driver?)
[    2.572437] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
[    2.580744] CPU0: stopping
[    2.583468] CPU: 0 PID: 0 Comm: swapper/0 Not tainted 4.4.84-00039-g845ce97-dirty #1
[    2.591244] Hardware name: Generic DRA74X (Flattened Device Tree)
[    2.597362] Backtrace: 
[    2.599840] [<c00131d4>] (dump_backtrace) from [<c00133d0>] (show_stack+0x18/0x1c)
[    2.607441]  r7:c08f5ef0 r6:20000193 r5:00000000 r4:c0913690
[    2.613169] [<c00133b8>] (show_stack) from [<c02b21a8>] (dump_stack+0x8c/0xa0)
[    2.620428] [<c02b211c>] (dump_stack) from [<c0016520>] (handle_IPI+0x184/0x198)
[    2.627852]  r7:c08f5ef0 r6:00000000 r5:00000000 r4:c08f0424
[    2.633575] [<c001639c>] (handle_IPI) from [<c00094c4>] (gic_handle_irq+0x78/0x7c)
[    2.641175]  r7:fa212000 r6:c08f5ef0 r5:fa21200c r4:c08f68ec
[    2.646895] [<c000944c>] (gic_handle_irq) from [<c0013ec0>] (__irq_svc+0x40/0x74)
[    2.654409] Exception stack(0xc08f5ef0 to 0xc08f5f38)
[    2.659484] 5ee0:                                     00000001 00000000 fe600000 00000000
[    2.667699] 5f00: c08f4000 c08f64ac 00000000 00000000 c08f5f60 c065e26c c08f650c c08f5f4c
[    2.675913] 5f20: c08f5f2c c08f5f40 c0027fec c0010600 60000013 ffffffff
[    2.682552]  r9:c065e26c r8:c08f5f60 r7:c08f5f24 r6:ffffffff r5:60000013 r4:c0010600
[    2.690383] [<c00105d8>] (arch_cpu_idle) from [<c0071468>] (default_idle_call+0x28/0x34)
[    2.698512] [<c0071440>] (default_idle_call) from [<c00716c8>] (cpu_startup_entry+0x200/0x260)
[    2.707170] [<c00714c8>] (cpu_startup_entry) from [<c0654d0c>] (rest_init+0x90/0x94)
[    2.714943]  r7:00000000
[    2.717501] [<c0654c7c>] (rest_init) from [<c089fd88>] (start_kernel+0x400/0x40c)
[    2.725012]  r5:c0943000 r4:c0943040
[    2.728622] [<c089f988>] (start_kernel) from [<80008090>] (0x80008090)
[    2.735176]  r10:00000000 r9:412fc0f2 r8:80007000 r7:c08fab38 r6:c08e0a24 r5:c08f6484
[    2.743079]  r4:c0943214
[    2.745636] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)












































U-Boot SPL 2016.05-00013-g3331a8a-dirty (Jun 03 2019 - 11:42:05)
DRA752-GP ES2.0
no pinctrl for hs200_1_8v
no pinctrl for ddr_1_8v
Trying to boot from MMC2_2
reading dra7-ipu2-fw.lzop
spl_load_file_fat: error reading file dra7-ipu2-fw.lzop, err - -1
spl: error reading image dra7-ipu2-fw.lzop, err - -1
Error loading remotecore IPU2!,Continuing with boot ...
reading dra7-dsp1-fw.lzop
spl_load_file_fat: error reading file dra7-dsp1-fw.lzop, err - -1
spl: error reading image dra7-dsp1-fw.lzop, err - -1
Error loading remotecore DSP1!,Continuing with boot ...
reading dra7-dsp2-fw.lzop
spl_load_file_fat: error reading file dra7-dsp2-fw.lzop, err - -1
spl: error reading image dra7-dsp2-fw.lzop, err - -1
Error loading remotecore DSP2!,Continuing with boot ...
reading dra7-ipu1-fw.lzop
spl_load_file_fat: error reading file dra7-ipu1-fw.lzop, err - -1
spl: error reading image dra7-ipu1-fw.lzop, err - -1
Error loading remotecore IPU1!,Continuing with boot ...
spl: falcon_args_file not set in environment, falling back to default
reading single-stage-boot.dtb
spl_load_image_fat_os: error reading image single-stage-boot.dtb, err - -1
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img


U-Boot 2016.05-00013-g3331a8a-dirty (Jun 03 2019 - 11:42:05 +0800)

CPU  : DRA752-GP ES2.0
Model: TI DRA742
Board: DRA74x EVM REV 
DRAM:  1.5 GiB
MMC:   i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
OMAP SD/MMC: 0, OMAP SD/MMC: 1
Warning: fastboot.board_rev: unknown board revision
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid GPT ***
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid Backup GPT ***
ERROR: cannot find partition: 'userdata'

at arch/arm/cpu/armv7/omap-common/utils.c:199/mmc_get_part_size()
Warning: fastboot.userdata_size: unable to calc
SCSI:  SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst 
scanning bus for devices...
Found 0 device(s).
Net:   Could not get PHY for ethernet@48484000: addr 2
eth0: ethernet@48484000
Hit any key to stop autoboot:  2 
CTRL-A Z for help | 115200 8N1 | NOR | Minicom 2.7 | VT102 | Offline | ttyUSB0                                                                











































 0 
## Error: "board_findfdt" not defined
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
134 bytes read in 2 ms (65.4 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
3476592 bytes read in 28 ms (118.4 MiB/s)
107051 bytes read in 11 ms (9.3 MiB/s)
Booting from mmc1 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x350c70 ]
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   Loading Device Tree to 8ffe2000, end 8ffff22a ... OK
Using machid 0xfe6 from environment

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Initializing cgroup subsys cpuset
[    0.000000] Initializing cgroup subsys cpu
[    0.000000] Initializing cgroup subsys cpuacct
[    0.000000] Linux version 4.4.84-00039-g845ce97-dirty (wang@buaawkp) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #1 SMP PREEMPT 9
[    0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[    0.000000] Machine model: TI DRA742
[    0.000000] Reserved memory: created DMA memory pool at 0x0000000040300000, size 3 MiB
[    0.000000] Reserved memory: initialized node cmem@40300000, compatible id shared-dma-pool
[    0.000000] Reserved memory: regions without no-map are not yet supported
[    0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 80 MiB
[    0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created CMA memory pool at 0x000000009e000000, size 32 MiB
[    0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: regions without no-map are not yet supported
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000a1000000, size 32 MiB
[    0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000a3000000, size 32 MiB
[    0.000000] Reserved memory: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: regions without no-map are not yet supported
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a9000000, size 32 MiB
[    0.000000] Reserved memory: initialized node cmem@A9000000, compatible id shared-dma-pool
[    0.000000] cma: Reserved 24 MiB at 0x00000000be400000
[    0.000000] Forcing write-allocate cache policy for SMP
[    0.000000] Memory policy: Data cache writealloc
[    0.000000] OMAP4: Map 0x00000000bfd00000 to fe600000 for dram barrier
[    0.000000] DRA752 ES2.0
[    0.000000] PERCPU: Embedded 11 pages/cpu @ef62a000 s14912 r8192 d21952 u45056
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 251456
[    0.000000] Kernel command line: console=ttyO0,115200n8 vram=16M root=/dev/mmcblk1p2 ip=none mem=1024M cm6
[    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Memory: 394396K/1012736K available (6479K kernel code, 309K rwdata, 2312K rodata, 340K init, 288K bss, 413540K reserved, 204800)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
[    0.000000]     vmalloc : 0xf0800000 - 0xff800000   ( 240 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xf0000000   ( 768 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc089e04c   (8793 kB)
[    0.000000]       .init : 0xc089f000 - 0xc08f4000   ( 340 kB)
[    0.000000]       .data : 0xc08f4000 - 0xc0941420   ( 310 kB)
[    0.000000]        .bss : 0xc0943000 - 0xc098b000   ( 288 kB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000]  Build-time adjustment of leaf fanout to 32.
[    0.000000] NR_IRQS:16 nr_irqs:16 16
[    0.000000] ti_dt_clocks_register: failed to lookup clock node gmac_gmii_ref_clk_div
[    0.000000] OMAP clockevent source: timer1 at 32786 Hz
[    0.000000] Architected cp15 timer(s) running at 6.14MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[    0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[    0.000016] Switching to timer-based delay loop, resolution 162ns
[    0.000339] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[    0.000347] OMAP clocksource: 32k_counter at 32768 Hz
[    0.000797] Console: colour dummy device 80x30
[    0.000812] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[    0.000818] This ensures that you still see kernel messages. Please
[    0.000823] update your kernel commandline.
[    0.000836] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[    0.000849] pid_max: default: 32768 minimum: 301
[    0.000946] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.000956] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.001496] Initializing cgroup subsys io
[    0.001512] Initializing cgroup subsys memory
[    0.001537] Initializing cgroup subsys devices
[    0.001549] Initializing cgroup subsys freezer
[    0.001559] Initializing cgroup subsys perf_event
[    0.001571] Initializing cgroup subsys pids
[    0.001597] CPU: Testing write buffer coherency: ok
[    0.001795] /cpus/cpu@0 missing clock-frequency property
[    0.001811] /cpus/cpu@1 missing clock-frequency property
[    0.001820] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.001857] Setting up static identity map for 0x80008380 - 0x800083e0
[    0.080061] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[    0.080130] Brought up 2 CPUs
[    0.080143] SMP: Total of 2 processors activated (24.59 BogoMIPS).
[    0.080149] CPU: All CPU(s) started in HYP mode.
[    0.080154] CPU: Virtualization extensions available.
[    0.080529] devtmpfs: initialized
[    0.109215] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[    0.110181] omap_hwmod: l3_main_2 using broken dt data from ocp
[    0.312561] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[    0.312582] futex hash table entries: 512 (order: 3, 32768 bytes)
[    0.316808] pinctrl core: initialized pinctrl subsystem
[    0.317662] NET: Registered protocol family 16
[    0.318571] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.340220] cpuidle: using governor ladder
[    0.370244] cpuidle: using governor menu
[    0.378761] OMAP GPIO hardware version 0.1
[    0.385218] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 !
[    0.401879] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[    0.401892] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[    0.409778] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[    0.409789] hw-breakpoint: maximum watchpoint size is 8 bytes.
[    0.410189] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[    0.410198] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[    0.410801] OMAP DMA hardware revision 0.0
[    0.451569] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[    0.452711] edma 43300000.edma: memcpy is disabled
[    0.457555] edma 43300000.edma: TI EDMA DMA engine driver
[    0.461928] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[    0.462103] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[    0.462259] omap-iommu 58882000.mmu: 58882000.mmu registered
[    0.462416] omap-iommu 55082000.mmu: 55082000.mmu registered
[    0.462701] omap-iommu 41501000.mmu: 41501000.mmu registered
[    0.462883] omap-iommu 41502000.mmu: 41502000.mmu registered
[    0.466196] palmas 0-0058: IRQ missing: skipping irq request
[    0.481323] palmas: probe of 0-0058 failed with error -121
[    0.481582] pcf857x: probe of 0-0020 failed with error -121
[    0.481830] pcf857x: probe of 0-0021 failed with error -121
[    0.481986] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[    0.482385] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
[    0.482570] media: Linux media interface: v0.10
[    0.482627] Linux video capture interface: v2.00
[    0.482666] pps_core: LinuxPPS API ver. 1 registered
[    0.482673] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.482697] PTP clock support registered
[    0.482744] EDAC MC: Ver: 3.0.0
[    0.483503] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[    0.483799] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[    0.484874] clocksource: Switched to clocksource arch_sys_counter
[    0.495211] NET: Registered protocol family 2
[    0.495696] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[    0.495759] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[    0.495884] TCP: Hash tables configured (established 8192 bind 8192)
[    0.495932] UDP hash table entries: 512 (order: 2, 16384 bytes)
[    0.495963] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[    0.496165] NET: Registered protocol family 1
[    0.496422] RPC: Registered named UNIX socket transport module.
[    0.496431] RPC: Registered udp transport module.
[    0.496437] RPC: Registered tcp transport module.
[    0.496443] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.497406] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[    0.507491] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.508145] NFS: Registering the id_resolver key type
[    0.508176] Key type id_resolver registered
[    0.508183] Key type id_legacy registered
[    0.508259] ntfs: driver 2.1.32 [Flags: R/O].
[    0.509515] bounce: pool size: 64 pages
[    0.509660] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[    0.509675] io scheduler noop registered
[    0.509686] io scheduler deadline registered
[    0.509718] io scheduler cfq registered (default)
[    0.514125] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
[    0.517383] PCI host bridge /ocp/axi@0/pcie_rc@51000000 ranges:
[    0.517396]   No bus range found for /ocp/axi@0/pcie_rc@51000000, using [bus 00-ff]
[    0.517429]    IO 0x20003000..0x20012fff -> 0x00000000
[    0.517449]   MEM 0x20013000..0x2fffffff -> 0x20013000
[    0.547312] dra7-pcie 51000000.pcie_rc: link is not up
[    0.547485] dra7-pcie 51000000.pcie_rc: PCI host bridge to bus 0000:00
[    0.547499] pci_bus 0000:00: root bus resource [bus 00-ff]
[    0.547509] pci_bus 0000:00: root bus resource [io  0x0000-0xffff]
[    0.547519] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[    0.547927] PCI: bus0: Fast back to back transfers disabled
[    0.548044] PCI: bus1: Fast back to back transfers enabled
[    0.548127] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[    0.548141] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[    0.548154] pci 0000:00:00.0: PCI bridge to [bus 01]
[    0.548371] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
[    0.608738] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[    0.612099] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 301, base_baud = 3000000) is a 8250
[    1.618502] console [ttyS0] enabled
[    1.622905] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 302, base_baud = 3000000) is a 8250
[    1.632611] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 303, base_baud = 3000000) is a 8250
[    1.642623] [drm] Initialized drm 1.1.0 20060810
[    1.648168] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    1.654812] [drm] No driver support for vblank timestamp query.
[    1.660984] [drm] Initialized vdrm 1.0.0 20110917 on minor 0
[    1.673722] loop: module loaded
[    1.677247] vmemexp device MAJOR num = 245
[    1.681376] vmemexp class registered
[    1.685109] /dev/vmemexp device registered
[    1.689224] ioctl DBUFIOC_EXPORT_VIRTMEM = -1072899120
[    1.694918] nand: No NAND device found
[    1.698689] omap2-nand 8000000.nand: scan failed, may be bus-width mismatch
[    1.708665] m25p80 spi32766.0: found s25fl512s, expected s25fl256s1
[    1.975994] m25p80 spi32766.0: s25fl512s (65536 Kbytes)
[    1.981305] 7 ofpart partitions found on MTD device spi32766.0
[    1.987182] Creating 7 MTD partitions on "spi32766.0":
[    1.992346] 0x000000000000-0x000000040000 : "QSPI.SPL"
[    1.998499] 0x000000040000-0x000000140000 : "QSPI.u-boot"
[    2.004846] 0x000000140000-0x0000001c0000 : "QSPI.u-boot-spl-os"
[    2.011816] 0x0000001c0000-0x0000001d0000 : "QSPI.u-boot-env"
[    2.017609] mtd: partition "QSPI.u-boot-env" doesn't end on an erase block -- force read-only
[    2.027103] 0x0000001d0000-0x0000001e0000 : "QSPI.u-boot-env.backup1"
[    2.033574] mtd: partition "QSPI.u-boot-env.backup1" doesn't start on an erase block boundary -- force read-only
[    2.054835] 0x0000001e0000-0x0000009e0000 : "QSPI.kernel"
[    2.060278] mtd: partition "QSPI.kernel" doesn't start on an erase block boundary -- force read-only
[    2.080390] 0x0000009e0000-0x000002000000 : "QSPI.file-system"
[    2.086269] mtd: partition "QSPI.file-system" doesn't start on an erase block boundary -- force read-only
[    2.098263] libphy: Fixed MDIO Bus: probed
[    2.144907] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
[    2.151032] davinci_mdio 48485000.mdio: detected phy mask fffffffe
[    2.159661] libphy: 48485000.mdio: probed
[    2.163693] davinci_mdio 48485000.mdio: phy[0]: device 48485000.mdio:00, driver unknown
[    2.172403] cpsw 48484000.ethernet: Detected MACID = 6c:c3:74:33:3c:6a
[    2.179087] cpsw 48484000.ethernet: cpts: overflow check period 800
[    2.186100] cpsw 48484000.ethernet: cpsw: Detected MACID = 6c:c3:74:33:3c:6b
[    2.194714] mousedev: PS/2 mouse device common for all mice
[    2.200907] i2c /dev entries driver
[    2.210248] omap_hsmmc 4809c000.mmc: Got CD GPIO
[    2.215904] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[    2.222288] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[    2.348850] ledtrig-cpu: registered to indicate activity on CPUs
[    2.356943] NET: Registered protocol family 10
[    2.362389] sit: IPv6 over IPv4 tunneling driver
[    2.368656] NET: Registered protocol family 17
[    2.373334] Key type dns_resolver registered
[    2.377740] omap_voltage_late_init: Voltage driver support not added
[    2.384644] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[    2.390872] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[    2.397126] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
[    2.403710] Power Management for TI OMAP4+ devices.
[    2.408840] Registering SWP/SWPB emulation handler
[    2.415076] dmm 4e000000.dmm: workaround for errata i878 in use
[    2.422656] dmm 4e000000.dmm: initialized all PAT entries
[    2.429119] [drm] Initialized omapdrm 1.0.0 20110917 on minor 1
[    2.436775] omap_hsmmc 4809c000.mmc: Got CD GPIO
[    2.442534] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[    2.448984] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[    2.455981] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[    2.462188] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[    2.468482] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
[    2.475499] hctosys: unable to open rtc device (rtc0)
[    2.492504] evm_1v8: disabling
[    2.495610] evm_3v3_sw: disabling
[    2.498940] aic_dvdd: disabling
[    2.502095] vmmcwl_fixed: disabling
[    2.505618] pbias_mmc_omap5: disabling
[    2.510582] VFS: Cannot open root device "mmcblk1p2" or unknown-block(0,0): error -6
[    2.518415] Please append a correct "root=" boot option; here are the available partitions:
[    2.526831] 1f00             256 mtdblock0  (driver?)
[    2.531918] 1f01            1024 mtdblock1  (driver?)
[    2.537027] 1f02             512 mtdblock2  (driver?)
[    2.542109] 1f03              64 mtdblock3  (driver?)
[    2.547215] 1f04              64 mtdblock4  (driver?)
[    2.552300] 1f05            8192 mtdblock5  (driver?)
[    2.557407] 1f06           22656 mtdblock6  (driver?)
[    2.562488] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
[    2.570796] CPU0: stopping
[    2.573521] CPU: 0 PID: 0 Comm: swapper/0 Not tainted 4.4.84-00039-g845ce97-dirty #1
[    2.581297] Hardware name: Generic DRA74X (Flattened Device Tree)
[    2.587415] Backtrace: 
[    2.589892] [<c00131d4>] (dump_backtrace) from [<c00133d0>] (show_stack+0x18/0x1c)
[    2.597493]  r7:c08f5ef0 r6:20000193 r5:00000000 r4:c0913690
[    2.603218] [<c00133b8>] (show_stack) from [<c02b21a8>] (dump_stack+0x8c/0xa0)
[    2.610476] [<c02b211c>] (dump_stack) from [<c0016520>] (handle_IPI+0x184/0x198)
[    2.617900]  r7:c08f5ef0 r6:00000000 r5:00000000 r4:c08f0424
[    2.623621] [<c001639c>] (handle_IPI) from [<c00094c4>] (gic_handle_irq+0x78/0x7c)
[    2.631220]  r7:fa212000 r6:c08f5ef0 r5:fa21200c r4:c08f68ec
[    2.636938] [<c000944c>] (gic_handle_irq) from [<c0013ec0>] (__irq_svc+0x40/0x74)
[    2.644454] Exception stack(0xc08f5ef0 to 0xc08f5f38)
[    2.649526] 5ee0:                                     00000001 00000000 fe600000 00000000
[    2.657742] 5f00: c08f4000 c08f64ac 00000000 00000000 c08f5f60 c065e26c c08f650c c08f5f4c
[    2.665953] 5f20: c08f5f2c c08f5f40 c0027fec c0010600 60000013 ffffffff
[    2.672592]  r9:c065e26c r8:c08f5f60 r7:c08f5f24 r6:ffffffff r5:60000013 r4:c0010600
[    2.680422] [<c00105d8>] (arch_cpu_idle) from [<c0071468>] (default_idle_call+0x28/0x34)
[    2.688551] [<c0071440>] (default_idle_call) from [<c00716c8>] (cpu_startup_entry+0x200/0x260)
[    2.697207] [<c00714c8>] (cpu_startup_entry) from [<c0654d0c>] (rest_init+0x90/0x94)
[    2.704981]  r7:00000000
[    2.707541] [<c0654c7c>] (rest_init) from [<c089fd88>] (start_kernel+0x400/0x40c)
[    2.715052]  r5:c0943000 r4:c0943040
[    2.718662] [<c089f988>] (start_kernel) from [<80008090>] (0x80008090)
[    2.725213]  r10:00000000 r9:412fc0f2 r8:80007000 r7:c08fab38 r6:c08e0a24 r5:c08f6484
[    2.733118]  r4:c0943214
[    2.735676] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)

CTRL-A Z for help | 115200 8N1 | NOR | Minicom 2.7 | VT102 | Offline | ttyUSB0                                                                

Does anyone help me solve this problem?

  • This is the schematic about emmc

  • Hi,

    I see this fragment in the log:

    [ 2.520529] VFS: Cannot open root device "mmcblk1p2" or unknown-block(0,0): error -6
    [ 2.528366] Please append a correct "root=" boot option; here are the available partitions:
    [ 2.536784] 1f00 256 mtdblock0 (driver?)
    [ 2.541870] 1f01 1024 mtdblock1 (driver?)
    [ 2.546979] 1f02 512 mtdblock2 (driver?)
    [ 2.552062] 1f03 64 mtdblock3 (driver?)
    [ 2.557166] 1f04 64 mtdblock4 (driver?)
    [ 2.562249] 1f05 8192 mtdblock5 (driver?)
    [ 2.567354] 1f06 22656 mtdblock6 (driver?)
    [ 2.572437] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)


    Can you try in the kernel command line to change "root=/dev/mmcblk1p2" to "root=/dev/mtdblock0" (I am not sure exactly which partition should be used) and see if it works?

    Regards,
    Yordan
  • Hi Yordan,

    Thank you for your reply.

    In the log file can see the mtdblk0-6 is aspirations flash,so I don't think it will work.  but I will try it

    Best regards

    Kepei

  • Hi Yordan,

    Thans for you suggestion!

    I had resolved the problem, there has some thing wrong in the schematic.

    Regards,

    Kepei