Part Number: AM3354
Should EMU1 (not EMU0) has to be pull-up during the power on even if ICEPICK is not required or used? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OK.
Actually there are pull-up on both EMU0 and EMU1.
Was it possible the EMU1 holding or stopping the processor booting-up if EMU1 got LOW?
By looking at the TRM, it seems not because they used by ICEPICK. Right? Thanks.
See Table 27-2 in the AM335x TRM Rev. P. EMU1=0 is not allowed and should not happen.