This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There are no sync outputs available from the chip.
Only sync on green is supported.
BR,
Steve
Shame!
What signals are really on pins AN9 and AM9? These are in my datasheet as VOUT[0]_VSYNC and HSYNC, and described as "Video Output 0 Vertical Sync output. This is the
discrete vertical synchronization output."
I'm getting more and more confused :(
Graeme,
These are sync outputs but for one of the digital out ports, not the analog DAC port.
There are 4 independent outputs...
1) HDMI/digital VOut[1]
2) HD DACs
3) Digital VOut[0]
4) SD DACs/RF output
Each output is completely independent of the others.
BR,
Steve
Thanks.
Do you rhink it is possible to run a digital output port at the same rate as an SD DAC output, AND have the syncs, er, in sync?
I see you mentioned the RF output pin. Are there any more details on this. My datasheet has this as RSVD.
This is something which has been discussed but not tried yet.
It is potentially possible to synchronize 2 video ports but until we actually try it I can't comment.
I think that the RF output has been de-specced.
BR,
Steve