Part Number: AM3358
Tool/software: Linux
how to apply patch to sdk linux kernel
sdk version : 5.00.02
kernel version : 4.14.
I have to apply 2 txt files as patch to linux kernel .
please guide me necessary steps
From linux-usb Fri Nov 20 22:13:07 2015
From: Bin Liu <b-liu () ti ! com>
Date: Fri, 20 Nov 2015 22:13:07 +0000
To: linux-usb
Subject: [PATCH RESEND v2 1/2] usb: phy: correct the am335x phy header filename
Message-Id: <1448057588-5358-1-git-send-email-b-liu () ti ! com>
X-MARC-Message: https://marc.info/?l=linux-usb&m=144805744319436
The filename of am35x-phy-control.h is confusing. The header is used
by the am335x phy driver, but the filename refers to am35x. Even worse
there is indeed another device called am35x but it does not use this
header at all.
Signed-off-by: Bin Liu <b-liu@ti.com>
---
v2: no change
drivers/usb/phy/phy-am335x-control.c | 2 +-
drivers/usb/phy/{am35x-phy-control.h => phy-am335x-control.h} | 0
drivers/usb/phy/phy-am335x.c | 2 +-
3 files changed, 2 insertions(+), 2 deletions(-)
rename drivers/usb/phy/{am35x-phy-control.h => phy-am335x-control.h} (100%)
diff --git a/drivers/usb/phy/phy-am335x-control.c b/drivers/usb/phy/phy-am335x-control.c
index 7b3035f..23fca51 100644
--- a/drivers/usb/phy/phy-am335x-control.c
+++ b/drivers/usb/phy/phy-am335x-control.c
@@ -4,7 +4,7 @@
#include <linux/of.h>
#include <linux/io.h>
#include <linux/delay.h>
-#include "am35x-phy-control.h"
+#include "phy-am335x-control.h"
struct am335x_control_usb {
struct device *dev;
diff --git a/drivers/usb/phy/am35x-phy-control.h b/drivers/usb/phy/phy-am335x-control.h
similarity index 100%
rename from drivers/usb/phy/am35x-phy-control.h
rename to drivers/usb/phy/phy-am335x-control.h
diff --git a/drivers/usb/phy/phy-am335x.c b/drivers/usb/phy/phy-am335x.c
index 90b67a4..8b6139d 100644
--- a/drivers/usb/phy/phy-am335x.c
+++ b/drivers/usb/phy/phy-am335x.c
@@ -9,7 +9,7 @@
#include <linux/of.h>
#include <linux/of_address.h>
-#include "am35x-phy-control.h"
+#include "phy-am335x-control.h"
#include "phy-generic.h"
struct am335x_phy {
--
1.8.4
--
To unsubscribe from this list: send the line "unsubscribe linux-usb" in
the body of a message to majordomo@vger.kernel.org
More majordomo info at http://vger.kernel.org/majordomo-info.html
From linux-usb Tue Dec 08 16:31:50 2015
From: Bin Liu <b-liu () ti ! com>
Date: Tue, 08 Dec 2015 16:31:50 +0000
To: linux-usb
Subject: [[PATCH v3]] usb: phy: phy-am335x: bypass first VBUS sensing for host-only mode
Message-Id: <1449592310-28995-1-git-send-email-b-liu () ti ! com>
X-MARC-Message: https://marc.info/?l=linux-usb&m=144959233413958
To prevent VBUS contention, the am335x MUSB phy senses VBUS first before
transitioning to host mode. However, for host-only mode, VBUS could be
directly tied to 5V power rail which could prevent MUSB transitions to
host mode.
This change receives dr_mode of the controller then bypass the first
VBUS sensing for host-only mode, so that MUSB can work in host mode
event if VBUS is tied to 5V.
Signed-off-by: Bin Liu <b-liu@ti.com>
---
v3: correct module dependency in Kconfig
drivers/usb/phy/Kconfig | 1 +
drivers/usb/phy/phy-am335x-control.c | 14 +++++++++++---
drivers/usb/phy/phy-am335x-control.h | 8 +++++---
drivers/usb/phy/phy-am335x.c | 15 ++++++++++-----
4 files changed, 27 insertions(+), 11 deletions(-)
diff --git a/drivers/usb/phy/Kconfig b/drivers/usb/phy/Kconfig
index 155694c..c690474 100644
--- a/drivers/usb/phy/Kconfig
+++ b/drivers/usb/phy/Kconfig
@@ -66,6 +66,7 @@ config AM335X_PHY_USB
select USB_PHY
select AM335X_CONTROL_USB
select NOP_USB_XCEIV
+ select USB_COMMON
help
This driver provides PHY support for that phy which part for the
AM335x SoC.
diff --git a/drivers/usb/phy/phy-am335x-control.c b/drivers/usb/phy/phy-am335x-control.c
index 23fca51..42a1afe 100644
--- a/drivers/usb/phy/phy-am335x-control.c
+++ b/drivers/usb/phy/phy-am335x-control.c
@@ -4,6 +4,7 @@
#include <linux/of.h>
#include <linux/io.h>
#include <linux/delay.h>
+#include <linux/usb/otg.h>
#include "phy-am335x-control.h"
struct am335x_control_usb {
@@ -58,7 +59,8 @@ static void am335x_phy_wkup(struct phy_control *phy_ctrl, u32 id, bool on)
spin_unlock(&usb_ctrl->lock);
}
-static void am335x_phy_power(struct phy_control *phy_ctrl, u32 id, bool on)
+static void am335x_phy_power(struct phy_control *phy_ctrl, u32 id,
+ enum usb_dr_mode dr_mode, bool on)
{
struct am335x_control_usb *usb_ctrl;
u32 val;
@@ -80,8 +82,14 @@ static void am335x_phy_power(struct phy_control *phy_ctrl, u32 id, bool on)
val = readl(usb_ctrl->phy_reg + reg);
if (on) {
- val &= ~(USBPHY_CM_PWRDN | USBPHY_OTG_PWRDN);
- val |= USBPHY_OTGVDET_EN | USBPHY_OTGSESSEND_EN;
+ if (dr_mode == USB_DR_MODE_HOST) {
+ val &= ~(USBPHY_CM_PWRDN | USBPHY_OTG_PWRDN |
+ USBPHY_OTGVDET_EN);
+ val |= USBPHY_OTGSESSEND_EN;
+ } else {
+ val &= ~(USBPHY_CM_PWRDN | USBPHY_OTG_PWRDN);
+ val |= USBPHY_OTGVDET_EN | USBPHY_OTGSESSEND_EN;
+ }
} else {
val |= USBPHY_CM_PWRDN | USBPHY_OTG_PWRDN;
}
diff --git a/drivers/usb/phy/phy-am335x-control.h b/drivers/usb/phy/phy-am335x-control.h
index b96594d..e86b316 100644
--- a/drivers/usb/phy/phy-am335x-control.h
+++ b/drivers/usb/phy/phy-am335x-control.h
@@ -2,13 +2,15 @@
#define _AM335x_PHY_CONTROL_H_
struct phy_control {
- void (*phy_power)(struct phy_control *phy_ctrl, u32 id, bool on);
+ void (*phy_power)(struct phy_control *phy_ctrl, u32 id,
+ enum usb_dr_mode dr_mode, bool on);
void (*phy_wkup)(struct phy_control *phy_ctrl, u32 id, bool on);
};
-static inline void phy_ctrl_power(struct phy_control *phy_ctrl, u32 id, bool on)
+static inline void phy_ctrl_power(struct phy_control *phy_ctrl, u32 id,
+ enum usb_dr_mode dr_mode, bool on)
{
- phy_ctrl->phy_power(phy_ctrl, id, on);
+ phy_ctrl->phy_power(phy_ctrl, id, dr_mode, on);
}
static inline void phy_ctrl_wkup(struct phy_control *phy_ctrl, u32 id, bool on)
diff --git a/drivers/usb/phy/phy-am335x.c b/drivers/usb/phy/phy-am335x.c
index 8b6139d..39b424f 100644
--- a/drivers/usb/phy/phy-am335x.c
+++ b/drivers/usb/phy/phy-am335x.c
@@ -8,6 +8,7 @@
#include <linux/regulator/consumer.h>
#include <linux/of.h>
#include <linux/of_address.h>
+#include <linux/usb/of.h>
#include "phy-am335x-control.h"
#include "phy-generic.h"
@@ -16,13 +17,14 @@ struct am335x_phy {
struct usb_phy_generic usb_phy_gen;
struct phy_control *phy_ctrl;
int id;
+ enum usb_dr_mode dr_mode;
};
static int am335x_init(struct usb_phy *phy)
{
struct am335x_phy *am_phy = dev_get_drvdata(phy->dev);
- phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, true);
+ phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, am_phy->dr_mode, true);
return 0;
}
@@ -30,7 +32,7 @@ static void am335x_shutdown(struct usb_phy *phy)
{
struct am335x_phy *am_phy = dev_get_drvdata(phy->dev);
- phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, false);
+ phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, am_phy->dr_mode, false);
}
static int am335x_phy_probe(struct platform_device *pdev)
@@ -46,12 +48,15 @@ static int am335x_phy_probe(struct platform_device *pdev)
am_phy->phy_ctrl = am335x_get_phy_control(dev);
if (!am_phy->phy_ctrl)
return -EPROBE_DEFER;
+
am_phy->id = of_alias_get_id(pdev->dev.of_node, "phy");
if (am_phy->id < 0) {
dev_err(&pdev->dev, "Missing PHY id: %d\n", am_phy->id);
return am_phy->id;
}
+ am_phy->dr_mode = of_usb_get_dr_mode_by_phy(pdev->dev.of_node);
+
ret = usb_phy_gen_create_phy(dev, &am_phy->usb_phy_gen, NULL);
if (ret)
return ret;
@@ -75,7 +80,7 @@ static int am335x_phy_probe(struct platform_device *pdev)
*/
device_set_wakeup_enable(dev, false);
- phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, false);
+ phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, am_phy->dr_mode, false);
return 0;
}
@@ -105,7 +110,7 @@ static int am335x_phy_suspend(struct device *dev)
if (device_may_wakeup(dev))
phy_ctrl_wkup(am_phy->phy_ctrl, am_phy->id, true);
- phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, false);
+ phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, am_phy->dr_mode, false);
return 0;
}
@@ -115,7 +120,7 @@ static int am335x_phy_resume(struct device *dev)
struct platform_device *pdev = to_platform_device(dev);
struct am335x_phy *am_phy = platform_get_drvdata(pdev);
- phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, true);
+ phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, am_phy->dr_mode, true);
if (device_may_wakeup(dev))
phy_ctrl_wkup(am_phy->phy_ctrl, am_phy->id, false);
--
1.9.1
--
To unsubscribe from this list: send the line "unsubscribe linux-usb" in
the body of a message to majordomo@vger.kernel.orgUntitled Document
More majordomo info at http://vger.kernel.org/majordomo-info.html