This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5708: Processor selection

Part Number: AM5708
Other Parts Discussed in Thread: DRA726, AM5728, AM5718, TMDXIDK5718, TMDSEVM572X

Hi All,

I need your advice for a single board computer application  which manages the HMI Touch Screen display.

I sent to Rogerio in private email the confidential block diagram of this application.

The first socket to define is the processor.

Main specs for the processor to look at are:

 Linux Operating System

  • Graphic Accelerator for the Play-Video feature to support HTML5 in full HD
  • Multi-Core if possible
  • 512Mb RAM
  • 2-4Gb Flash, better if scalable (1Gb RAM, 8Gb Flash for the performance solution)
  • Communication Interfaces:

5x UART (1x debug for Linux Console)

1x 10/100/1000 Mb Ethernet

2x I2X

2x USB 2.0

Able to manage a WiFi-BLE module

2x CAN Bus (data rate up to 1Mbit/s), better if separated: 1 for internal peripherals and the other one for external modules

1x SPI for Touch Screen

1x LVDS/HDMI/RGB

1x Analog Audio Output (Optional)

One of the main spec is to have the OS Linux. Indeed customer was using NXP platform i.MX 8 and 6 series but the Chromium browser did not support the graphic and video accelerators. In particular GPU (Graphic) was supported but not the VPU (Video).

 

Could you please recommend me any processor that might fit the above specs? Also any TIDesign or AppNote could be interesting.

I was thinking at SITARA AM5708 or even DRA726.

Are you aware whether our processor AM5708 might support the above specs?

Many Thanks,

Antonio