Part Number: TMS320C6657
Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
Hi,
I'm not getting console output when I call the DbgPrintf function while running the NDK 3.40.1.01 on an EVMC6657L board.
I'm using SYSBIOS 6.75.2.00
XDC 3.50.8.24_core
I've set the debug print level to DBG_INFO in the stack configuration task:
rc = DBG_INFO;
CfgAddEntry (hCfg, CFGTAG_OS, CFGITEM_OS_DBGPRINTLEVEL,
CFG_ADDMODE_UNIQUE, sizeof(uint32_t), (UINT8 *) &rc, 0);
I've also tried just calling System_printf( ) directly, from main() and also from a task. If I simply call the printf() function, I do see the output on the console. The console, is viewed through the jtag emulator:
My SYSBIOS configuration file is pasted below. I'd appreciate some help in getting this functionality working.
Thanks,
Jim
var Defaults = xdc.useModule('xdc.runtime.Defaults');
var Diags = xdc.useModule('xdc.runtime.Diags');
var Error = xdc.useModule('xdc.runtime.Error');
var Log = xdc.useModule('xdc.runtime.Log');
var LoggerBuf = xdc.useModule('xdc.runtime.LoggerBuf');
var Main = xdc.useModule('xdc.runtime.Main');
var Memory = xdc.useModule('xdc.runtime.Memory')
var SysMin = xdc.useModule('xdc.runtime.SysMin');
var System = xdc.useModule('xdc.runtime.System');
var Text = xdc.useModule('xdc.runtime.Text');
var BIOS = xdc.useModule('ti.sysbios.BIOS');
var Clock = xdc.useModule('ti.sysbios.knl.Clock');
var Swi = xdc.useModule('ti.sysbios.knl.Swi');
var Task = xdc.useModule('ti.sysbios.knl.Task');
var Semaphore = xdc.useModule('ti.sysbios.knl.Semaphore');
var Hwi = xdc.useModule('ti.sysbios.hal.Hwi');
var Idle = xdc.useModule('ti.sysbios.knl.Idle');
var Timer = xdc.useModule('ti.sysbios.timers.timer64.Timer');
var Timestamp = xdc.useModule('xdc.runtime.Timestamp');
var Cache = xdc.useModule('ti.sysbios.family.c66.Cache');
/* lower half of DDR3 is cached */
Cache.setMarMeta(0x80000000, 0x10000000, 1);
/* upper half of DDR3 is non-cached */
Cache.setMarMeta(0x90000000, 0x10000000, 0);
var Exception = xdc.useModule('ti.sysbios.family.c64p.Exception');
var CpIntc = xdc.useModule('ti.sysbios.family.c66.tci66xx.CpIntc');
var EventCombiner = xdc.useModule('ti.sysbios.family.c64p.EventCombiner');
var HeapMem = xdc.useModule('ti.sysbios.heaps.HeapMem');
var HeapBuf = xdc.useModule('ti.sysbios.heaps.HeapBuf');
/*
** Use this load to configure NDK 2.2 and above using RTSC. In previous versions of
** the NDK RTSC configuration was not supported and you should comment this out.
*/
var Ndk = xdc.loadPackage('ti.ndk.config');
var Global = xdc.useModule('ti.ndk.config.Global');
/*
** This allows the heart beat (poll function) to be created but does not generate the stack threads
**
** Look in the cdoc (help files) to see what CfgAddEntry items can be configured. We tell it NOT
** to create any stack threads (services) as we configure those ourselves in our Main Task
** thread hpdspuaStart.
*/
Global.enableCodeGeneration = false;
var Startup = xdc.useModule('xdc.runtime.Startup');
var SysStd = xdc.useModule('xdc.runtime.SysStd');
/*
* Uncomment this line to globally disable Asserts.
* All modules inherit the default from the 'Defaults' module. You
* can override these defaults on a per-module basis using Module.common$.
* Disabling Asserts will save code space and improve runtime performance.
Defaults.common$.diags_ASSERT = Diags.ALWAYS_OFF;
*/
/*
* Uncomment this line to keep module names from being loaded on the target.
* The module name strings are placed in the .const section. Setting this
* parameter to false will save space in the .const section. Error and
* Assert messages will contain an "unknown module" prefix instead
* of the actual module name.
Defaults.common$.namedModule = false;
*/
/*
* Minimize exit handler array in System. The System module includes
* an array of functions that are registered with System_atexit() to be
* called by System_exit().
*/
System.maxAtexitHandlers = 8;
/*
* Uncomment this line to disable the Error print function.
* We lose error information when this is disabled since the errors are
* not printed. Disabling the raiseHook will save some code space if
* your app is not using System_printf() since the Error_print() function
* calls System_printf().
Error.raiseHook = null;
*/
/*
* Uncomment this line to keep Error, Assert, and Log strings from being
* loaded on the target. These strings are placed in the .const section.
* Setting this parameter to false will save space in the .const section.
* Error, Assert and Log message will print raw ids and args instead of
* a formatted message.
Text.isLoaded = false;
*/
/*
* Uncomment this line to disable the output of characters by SysMin
* when the program exits. SysMin writes characters to a circular buffer.
* This buffer can be viewed using the SysMin Output view in ROV.
SysMin.flushAtExit = false;
*/
/*
* The BIOS module will create the default heap for the system.
* Specify the size of this default heap.
*/
BIOS.heapSize = 0x1000;
/*
* Build a custom SYS/BIOS library from sources.
*/
BIOS.libType = BIOS.LibType_Custom;
/* System stack size (used by ISRs and Swis) */
Program.stack = 0x2000;
/* Circular buffer size for System_printf() */
SysMin.bufSize = 0x200;
/*
* Create and install logger for the whole system
*/
var loggerBufParams = new LoggerBuf.Params();
loggerBufParams.numEntries = 16;
var logger0 = LoggerBuf.create(loggerBufParams);
Defaults.common$.logger = logger0;
Main.common$.diags_INFO = Diags.ALWAYS_ON;
System.SupportProxy = SysMin;
var clock0Params = new Clock.Params();
clock0Params.instance.name = "clock0";
clock0Params.period = 1;
clock0Params.startFlag = true;
Program.global.clock0 = Clock.create("&GpakSchedulingTimer", 1, clock0Params);
Idle.idleFxns[0] = "&GpakIdleTaskFunc";
var HeapMem = xdc.useModule('ti.sysbios.heaps.HeapMem');
var heapMemParams = new HeapMem.Params();
heapMemParams.size = 0x8000;
heapMemParams.sectionName = "systemHeap";
Program.global.heap0 = HeapMem.create(heapMemParams);
Memory.defaultHeapInstance = Program.global.heap0;
Program.sectMap["sharedL2"] = "MSMCSRAM";
Program.sectMap["systemHeap"] = "MSMCSRAM";
Program.sectMap[".sysmem"] = "MSMCSRAM";
Program.sectMap[".args"] = "MSMCSRAM";
Program.sectMap[".cio"] = "MSMCSRAM";
Program.sectMap[".far"] = "MSMCSRAM";
/*
Program.sectMap[".rodata"] = "MSMCSRAM";
Program.sectMap[".neardata"] = "MSMCSRAM";
Program.sectMap[".bss"] = "MSMCSRAM";
*/
Program.sectMap[".cppi"] = "MSMCSRAM";
Program.sectMap[".init_array"] = "MSMCSRAM";
Program.sectMap[".qmss"] = "MSMCSRAM";
Program.sectMap[".cinit"] = "MSMCSRAM";
Program.sectMap[".const"] = "MSMCSRAM";
Program.sectMap[".text"] = "MSMCSRAM";
Program.sectMap[".code"] = "MSMCSRAM";
Program.sectMap[".switch"] = "MSMCSRAM";
Program.sectMap[".data"] = "MSMCSRAM";
Program.sectMap[".fardata"] = "MSMCSRAM";
Program.sectMap[".args"] = "MSMCSRAM";
Program.sectMap[".cio"] = "MSMCSRAM";
Program.sectMap[".vecs"] = "MSMCSRAM";
Program.sectMap["emacComm"] = "L2SRAM"
Program.sectMap[".far:taskStackSection"] = "L2SRAM";
Program.sectMap[".stack"] = "L2SRAM";
Program.sectMap[".far:IMAGEDATA"] = {loadSegment: "L2SRAM", loadAlign: 8};
Program.sectMap[".far:NDK_OBJMEM"] = {loadSegment: "L2SRAM", loadAlign: 8};
Program.sectMap[".far:NDK_PACKETMEM"] = {loadSegment: "L2SRAM", loadAlign: 128};
/* Load the CSL package */
var devType = "c6657";
var Csl = xdc.useModule('ti.csl.Settings');
Csl.deviceType = devType;
Csl.useCSLIntcLib = true;
/* Load the OSAL package */
var osType = "tirtos"
var Osal = xdc.useModule('ti.osal.Settings');
Osal.osType = osType;
/* Load the QMSS package */
var Qmss = xdc.loadPackage('ti.drv.qmss');
/* Load the EMAC packages */
var Emac = xdc.loadPackage('ti.drv.emac');
Emac.Settings.socType = devType;
var socType = "c6657";
var Nimu = xdc.loadPackage('ti.transport.ndk.nimu');
Nimu.Settings.socType = socType;