This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSICE3359: ICEv2 factory settings

Part Number: TMDSICE3359
Other Parts Discussed in Thread: AM3359

Hello, I 've few question :

-What is the Kernel of AM3359? (Is it a Linux RT, Linux or TI-RTOS kernel?)

-And what is the pre installed Operating System on this processor?

-And I need to change the OS of this processor if we use the Processor SDK Linux RT, the Processor SDK Linux or the Processor SDK RTOS?

Thanks.

Best regards,

Florian

  • Hi,

    user5993022 said:
    What is the Kernel of AM3359? (Is it a Linux RT, Linux or TI-RTOS kernel?)

    All of these are available for AM335x devices.

    user5993022 said:
    And what is the pre installed Operating System on this processor?

    AM335x does not have internal flash memory, so there is no OS preinstalled. If you are asking about the ICEv2 EVM board, it is shipped with the EtherCAT Slave demo, based on TI-RTOS. This is installed in the SPI flash on the board.

    user5993022 said:
    And I need to change the OS of this processor if we use the Processor SDK Linux RT, the Processor SDK Linux or the Processor SDK RTOS?

    Yes, for boot configuration please refer to section 4 in