Part Number: TDA2SX
Other Parts Discussed in Thread: DRA742, PMP
Tool/software: Linux
Dear TI,
I am now trying to flashing eMMC over USB interface.
My operations:
step1: host$ sudo ./usbboot -S spl/u-boot-spl.bin
step2: set sw2[7:0] at cpu board as [0 0 0 0 0 0 0 0], and then power on the evm.
host machine output:
reading ASIC ID
CHIP: 5641
rom minor version: 02
IDEN: 0000000000000000000000000000000000000000
MPKH: 0000000000000000000000000000000000000000000000000000000000000000
CRC0: 51d2f9a7
CRC1: 00000000
device is GP
sending 2ndstage to target...
evm output:
U-Boot SPL 2016.05-00008-g1fbee98-dirty (Jun 06 2019 - 20:35:16)
DRA752-GP ES2.0
Trying to boot from USB DFU
Using default environment
UNKNOWN IRQ type 1715168365 <----------------------It looks like an USB IRQ error showing from the code, but i don't know why.
step3: host$ sudo dfu-util -l
dfu-util 0.9
Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2016 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to sourceforge.net/.../
Found DFU: [0451:d022] ver=0223, devnum=38, cfg=1, intf=0, path="1-7", alt=2, name="ramdisk", serial="UNKNOWN"
Found DFU: [0451:d022] ver=0223, devnum=38, cfg=1, intf=0, path="1-7", alt=1, name="fdt", serial="UNKNOWN"
Found DFU: [0451:d022] ver=0223, devnum=38, cfg=1, intf=0, path="1-7", alt=0, name="kernel", serial="UNKNOWN"
step4: host$ sudo dfu-util -D boot.img -c 1 -i 0 -a 0
dfu-util 0.9
Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2016 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to sourceforge.net/.../
dfu-util: File size is too big: Success
The file boot.img was generated by issue:
dd if=/dev/sdb1 of=boot.img bs=1M count=4096 &
dd if=/dev/sdb2 of=boot.img bs=1m count=4096 &
/dev/sdb1 & /dev/sdb2 are my bootable SD card device. I just replaced uenv.txt in the boot partition with uenv-emmc.txt.
step5: host$ sudo dfu-util -D u-boot.img -c 1 -i 0 -a 0 -R <-----------------------------------------I try to debug the problem show in step 4.
dfu-util 0.9
Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2016 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to sourceforge.net/.../
dfu-util: Invalid DFU suffix signature
dfu-util: A valid DFU suffix will be required in a future dfu-util release!!!
Opening DFU capable USB device...
ID 0451:d022
Run-time device DFU version 0110
Claiming USB DFU Interface...
Setting Alternate Setting #0 ...
Determining device status: state = dfuIDLE, status = 0
dfuIDLE, continuing
DFU mode device DFU version 0110
Device returned transfer size 4096
Copying data from PC to DFU device
Download [=========================] 100% 837964 bytes
Download done.
state(7) = dfuMANIFEST, status(0) = No error condition is present
state(2) = dfuIDLE, status(0) = No error condition is present
Done!
step 6: target output:
U-Boot 2016.05-00008-g1fbee98-dirty (Jun 06 2019 - 20:35:16 +0800)
CPU : DRA752-GP ES2.0
Model: TI DRA742
Board: DRA74x EVM REV H.0
DRAM: 4 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
** First descriptor is NOT a primary desc on 1:1 **
*** Warning - bad CRC, using default environment
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid GPT ***
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid Backup GPT ***
ERROR: cannot find partition: 'userdata'
at arch/arm/cpu/armv7/omap-common/utils.c:195/mmc_get_part_size()
Warning: fastboot.userdata_size: unable to calc
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net:
Warning: ethernet@48484000 using MAC address from ROM
eth0: ethernet@48484000
Hit any key to stop autoboot: 0
=>
step7: uboot $ printenv
=> printenv
arch=arm
args_fit=setenv bootargs console=${console}
args_mmc=run finduuid;setenv bootargs console=${console} ${optargs} root=PARTUUID=${uuid} rw rootfstype=${mmcrootfstype}
baudrate=115200
board=dra7xx
board_name=dra7xx
board_rev=H.0
boot_fdt=try
boot_fit=0
boot_os=0
bootargs=androidboot.serialno=${serial#} console=ttyS0,115200 androidboot.console=ttyS0 androidboot.hardware=jacinto6evmboard
bootcmd=if test ${dofastboot} -eq 1; then echo Boot fastboot requested, resetting dofastboot ...;setenv dofastboot 0; saveenv;echo Booting into fastboot ...; fastboot 0; fi;if test ${boot_fit} -eq 1; then run update_to_fit;fi;run findfdt; run envboot; run mmcboot;run emmc_android_boot;
bootdelay=2
bootdir=/boot
bootenvfile=uEnv.txt
bootfile=zImage
bootm_size=0x10000000
bootpart=0:2
bootscript=echo Running bootscript from mmc${mmcdev} ...; source ${loadaddr}
console=ttyO0,115200n8
cpu=armv7 --------------------------------------------------------The size of boot.img is 4GB, so i modify the rawemmc raw parameters. I don't know whether it's right or not.
dfu_alt_info_emmc=rawemmc raw 0 4294967296;boot part 1 1;rootfs part 1 2;MLO fat 1 1;MLO.raw raw 0x100 0x100;u-boot.img.raw raw 0x300 0x1000;u-env.raw raw 0x1300 0x200;spl-os-args.raw raw 0x1500 0x200;spl-os-image.raw raw 0x1700 0x6900;spl-os-args fat 1 1;spl-os-image fat 1 1;u-boot.img fat 1 1;uEnv.txt fat 1 1
dfu_alt_info_mmc=boot part 0 1;rootfs part 0 2;MLO fat 0 1;MLO.raw raw 0x100 0x100;u-boot.img.raw raw 0x300 0x1000;u-env.raw raw 0x1300 0x200;spl-os-args.raw raw 0x1500 0x200;spl-os-image.raw raw 0x1700 0x6900;spl-os-args fat 0 1;spl-os-image fat 0 1;u-boot.img fat 0 1;uEnv.txt fat 0 1
dfu_alt_info_qspi=MLO raw 0x0 0x040000;u-boot.img raw 0x040000 0x0100000;u-boot-spl-os raw 0x140000 0x080000;u-boot-env raw 0x1C0000 0x010000;u-boot-env.backup raw 0x1D0000 0x010000;kernel raw 0x1E0000 0x800000
dfu_alt_info_ram=kernel ram 0x80200000 0x4000000;fdt ram 0x80f80000 0x80000;ramdisk ram 0x81000000 0x4000000
dfu_bufsiz=0x10000
dofastboot=0
emmc_android_boot=setenv eval_bootargs setenv bootargs $bootargs; run eval_bootargs; setenv mmcdev 1; setenv fdt_part 3; setenv boot_part 9; if test $reboot_image = recovery; then setenv boot_part 8; setenv reboot_image boot; saveenv; fi;setenv machid fe6; mmc dev $mmcdev; mmc rescan; part start mmc ${mmcdev} ${fdt_part} fdt_start; part size mmc ${mmcdev} ${fdt_part} fdt_size; part start mmc ${mmcdev} ${boot_part} boot_start; part size mmc ${mmcdev} ${boot_part} boot_size; mmc read ${fdtaddr} ${fdt_start} ${fdt_size}; mmc read ${loadaddr} ${boot_start} ${boot_size}; echo Booting from eMMC ...; bootm $loadaddr $loadaddr $fdtaddr;
envboot=mmc dev ${mmcdev}; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadbootscript; then run bootscript;else if run loadbootenv; then echo Loaded env from ${bootenvfile};run importbootenv;fi;if test -n $uenvcmd; then echo Running uenvcmd ...;run uenvcmd;fi;fi;fi;
ethaddr=0c:b2:b7:f6:ff:bc
fastboot.board_rev=H.0
fastboot.cpu=J6
fastboot.secure=GP
fastboot.userdata_size=unknown
fdt_addr_r=0x88000000
fdtaddr=0x88000000
fdtcontroladdr=fdf0a598
fdtfile=undefined
findfdt=if test $board_name = omap5_uevm; then setenv fdtfile omap5-uevm.dtb; fi; if test $board_name = dra7xx; then setenv fdtfile dra7-evm.dtb; fi;if test $board_name = dra72x-revc; then setenv fdtfile dra72-evm-revc.dtb; fi;if test $board_name = dra72x; then setenv fdtfile dra72-evm.dtb; fi;if test $board_name = dra71x; then setenv fdtfile dra71-evm.dtb; fi;if test $board_name = dra76x; then setenv fdtfile dra76-evm.dtb; fi;if test $board_name = beagle_x15; then setenv fdtfile am57xx-beagle-x15.dtb; fi;if test $board_name = beagle_x15_revb1; then setenv fdtfile am57xx-beagle-x15-revb1.dtb; fi;if test $board_name = am57xx_evm; then setenv fdtfile am57xx-evm.dtb; fi;if test $board_name = am57xx_evm_reva3; then setenv fdtfile am57xx-evm-reva3.dtb; fi;if test $board_name = am572x_idk && test $idk_lcd = no; then setenv fdtfile am572x-idk.dtb; fi;if test $board_name = am572x_idk && test $idk_lcd = osd101t2045; then setenv fdtfile am572x-idk-lcd-osd.dtb; fi;if test $board_name = am572x_idk && test $idk_lcd = osd101t2587; then setenv fdtfile am572x-idk-lcd-osd101t2587.dtb; fi;if test $board_name = am571x_idk && test $idk_lcd = no; then setenv fdtfile am571x-idk.dtb; fi;if test $board_name = am571x_idk && test $idk_lcd = osd101t2045; then setenv fdtfile am571x-idk-lcd-osd.dtb; fi;if test $board_name = am571x_idk && test $idk_lcd = osd101t2587; then setenv fdtfile am571x-idk-lcd-osd101t2587.dtb; fi;if test $fdtfile = undefined; then echo WARNING: Could not determine device tree to use; fi;
finduuid=part uuid mmc ${bootpart} uuid
fit_bootfile=fitImage.itb
fit_loadaddr=0x88000000
importbootenv=echo Importing environment from mmc${mmcdev} ...; env import -t ${loadaddr} ${filesize}
kernel_addr_r=0x82000000
loadaddr=0x82000000
loadbootenv=fatload mmc ${mmcdev} ${loadaddr} ${bootenvfile}
loadbootscript=fatload mmc ${mmcdev} ${loadaddr} boot.scr
loadfdt=load ${devtype} ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile}
loadfit=run args_fit; bootm ${loadaddr}#${fdtfile};
loadimage=load mmc ${bootpart} ${loadaddr} ${bootdir}/${bootfile}
mmcboot=if mmc dev ${mmcdev}; then setenv devtype mmc; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadimage; then run loadfdt; echo Booting from mmc${mmcdev} ...; run args_mmc; bootz ${loadaddr} - ${fdtaddr}; fi; fi; fi;
mmcdev=0
mmcloados=run args_mmc; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdtaddr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;
mmcrootfstype=ext4 rootwait
netargs=setenv bootargs console=${console} ${optargs} root=/dev/nfs nfsroot=${serverip}:${rootpath},${nfsopts} rw ip=dhcp
netboot=echo Booting from network ...; setenv autoload no; dhcp; run netloadimage; run netloadfdt; run netargs; bootz ${loadaddr} - ${fdtaddr}
netloadfdt=tftp ${fdtaddr} ${fdtfile}
netloadimage=tftp ${loadaddr} ${bootfile}
nfsopts=nolock
partitions=uuid_disk=${uuid_gpt_disk};name=rootfs,start=2MiB,size=-,uuid=${uuid_gpt_rootfs}
partitions_android=uuid_disk=${uuid_gpt_disk};name=xloader,start=128K,size=256K,uuid=${uuid_gpt_xloader};name=bootloader,size=2304K,uuid=${uuid_gpt_bootloader};name=environment,size=256K,uuid=${uuid_gpt_environment};name=misc,size=128K,uuid=${uuid_gpt_misc};name=reserved,size=384K,uuid=${uuid_gpt_reserved};name=efs,size=16M,uuid=${uuid_gpt_efs};name=crypto,size=16K,uuid=${uuid_gpt_crypto};name=recovery,size=10M,uuid=${uuid_gpt_recovery};name=boot,size=10M,uuid=${uuid_gpt_boot};name=system,size=768M,uuid=${uuid_gpt_system};name=vendor,size=256M,uuid=${uuid_gpt_vendor};name=cache,size=256M,uuid=${uuid_gpt_cache};name=ipu1,size=8M,uuid=${uuid_gpt_ipu1};name=ipu2,size=8M,uuid=${uuid_gpt_ipu2};name=dsp1,size=8M,uuid=${uuid_gpt_dsp1};name=dsp2,size=8M,uuid=${uuid_gpt_dsp2};name=userdata,size=-,uuid=${uuid_gpt_userdata}
pxefile_addr_r=0x80100000
ramdisk_addr_r=0x88080000
rdaddr=0x88080000
reboot_image=boot
rootpath=/export/rootfs
scriptaddr=0x80000000
scsidevs=0
serial#=0400d00f147400e2
soc=omap5
static_ip=${ipaddr}:${serverip}:${gatewayip}:${netmask}:${hostname}::off
stderr=serial@4806a000
stdin=serial@4806a000
stdout=serial@4806a000
update_to_fit=setenv loadaddr ${fit_loadaddr}; setenv bootfile ${fit_bootfile}
usbtty=cdc_acm
vendor=ti
ver=U-Boot 2016.05-00008-g1fbee98-dirty (Jun 06 2019 - 20:35:16 +0800)
vram=16M
Environment size: 7479/131067 bytes
=>
That's all what i have done.
I want to know what can i do next to make eMMC flashed successful over DFU tools?
Regards,
Liu Gan