This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux: Custom kernel module

Tool/software: Linux

Hello.

I have some am335x-evm board. For work something software I need kernel modules, which are not included to current board software.

I see, that version of kernel is:

root@am335x-evm:~# opkg list-installed | grep kernel-3.12
kernel-3.12.10-ti2013.12.01 - 3.12.10-r21k+gitrAUTOINC+2325bb5680986b6914d8fd0b5d0bdc20081fe8d3-arago6-amsdk2
root@am335x-evm:~#

When I try to install myself prepared (with arago-project.org bitbake) kernel modules I have error:

root@am335x-evm:~# opkg install kernel-module-esp4_3.12.10-r21k+gitrAUTOINC+2325bb5680-arago5.11_am335x_evm.ipk
Installing kernel-module-esp4 (3.12.10-r21k+gitrAUTOINC+2325bb5680-arago5.11) to root...
Collected errors:
 * satisfy_dependencies_for: Cannot satisfy the following dependencies for kernel-module-esp4:
 *      kernel-3.12.10-g2325bb5 *
 * opkg_install_cmd: Cannot install package kernel-module-esp4.
root@am335x-evm:~#

I see, that there is different kernels VERMAGIC string. Is there a way to prepare (with arago-project.org bitbake or some other way)

kernel modules with right VERMAGIC?