This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TMS320C6657: Need legacy C6657 MCSDK v2.01.02.06 Linux installer that includes C6657 PDK v1.1.2.6

Part Number: TMS320C6657

Tool/software: TI-RTOS

I have an older project that I am resurrecting for some work, and I need to get the C6657 PDK v1.1.2.6.  I believe this was included in the MCSDK v2.01.02.06 for the C6657.  I originally developed this on a Windows machine, so I only have the installer for Windows.  I tried copying the windows version of the PDK directory (which I saved) to Linux, but I get an error when trying to import it.

Operation details:
Cannot complete the install because some dependencies are not satisfiable
com.ti.biosmcsdk.pdk.C6657.p2.feature.group [1.1.2.6] cannot be installed in this environment because its filter is not applicable.

 

 Does anybody have a link to download this software package (linux variant).  

Thanks,

Mark