Part Number: PROCESSOR-SDK-TDAX
Tool/software: Linux
Am just trying to use Vision SDK for object recognition. Should it work without having the EVM kit or whether I can emulate the EVM kit.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PROCESSOR-SDK-TDAX
Tool/software: Linux
Am just trying to use Vision SDK for object recognition. Should it work without having the EVM kit or whether I can emulate the EVM kit.
Hi,
You need to have at least 1 support platform mentioned in released notes to run VSDK.
There are some individual package which comes as a part of VSDK which can be run on PC but for that you need to check the release notes or other related docs for that package/component.(OpenVx is an example of such package which can be ran on PC environment).
Regards,
Anuj
Hi,
No, It does not have GUI.
You have to control everything over UART console.
Regards,
Anuj