Part Number: AM5726
Hi,
The following is described in TRM 27.4.2.1 Synchronous Path: Interrupt Request Generation.
The general-purpose interface has 14 interrupt lines (two interrupt lines per GPIO module instance for
biprocessor operation for GPIO1 through GPIO6 and one interrupt line for GPIO7 and GPIO8 module
instance).
Even if I confirm below TRM, GPIO7 and GPIO8 have 2 interrupts each, and the total of GPIO has 16 interrupts.
Is the above description incorrect?
Figure 27-6. GPIO Integration
Table 17-13. Connection of Device IRQs to IRQ_CROSSBAR Inputs
Best Regards,
Shigehiro Tsuda