Other Parts Discussed in Thread: TPS65218,
Sitara support Team,
I would like to make sure about the Simplified Power Sequencing.
Q1. As described "Figure 5-8. " in the datasheet,
Is there no problem to use TPS65218D0RSL if 1.8V is set at any one of VDDSHVx?
Because our customer can set 1.8V to only VDDSHV5.
Q2. VDDSHV5 is described "supply voltage range for the CLKOUT voltage domain"
Is VDDSHV5 the power source with only D24 pin and C24 pin?
Or is there any other possibility of using this power source internally?
Best regards,
Kanae