This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interfacing the DM365 to a wireless card



Suppose I need to interface TI DM365 to a WLAN card,

which interface(s) can I use? I prefer mini-PCI, but it seems

DM365 does not support mini-PCI, correct?

 

I checked the DM365 manual, and it looks like it use SDIO to interface

to wireless. Can we use USB to interface to wireless?

  • ClayCope said:
    Suppose I need to interface TI DM365 to a WLAN card,
    which interface(s) can I use? I prefer mini-PCI, but it seems
    DM365 does not support mini-PCI, correct?

    This is true, the DM365 has no PCI interface, in general the solutions I have seen have been through either USB or SDIO using off the shelf WiFi solutions. The easiest way today would probably be to use a USB based WiFi solution, as SDIO support on the DM365 may not be around for some time, until a newer kernel support package is released. In general the USB WiFi driver would be provided by the manufacturer or could possibly be included in the kernel already, though I have not seen any particular WiFi adapters used on the DM365 to recommend there was a Belkin model used in this wiki article on prior Davinci devices.

  • Thanks for the reply and information. I have either a mini-PCI or PCI wifi card. Can I use the PCI-USB adapter to interface to the WiFi card with the DM365?

  • I have not come across such an adapter to provide a PCI slot from a USB interface, however this should be possible, though it will likely require additional driver development as it sounds like a somewhat unique configuration, in general the more standard your setup is the more likely it will work easily.