Part Number: AM5728
Tool/software: Linux
Hi:
Software version: ti-processor-sdk-linux-rt-am57xx-evm-03.03.00.04, hardware version: AM5728-ES2.0, custom board,
1, how to use the ltp tool?
2. Is there a tutorial on using the ltp tool.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM5728
Tool/software: Linux
Hi:
Software version: ti-processor-sdk-linux-rt-am57xx-evm-03.03.00.04, hardware version: AM5728-ES2.0, custom board,
1, how to use the ltp tool?
2. Is there a tutorial on using the ltp tool.
Hi:
1. How do I use ltp to test the file system in Linux?
/opt/ltp/runltp -f fs prompt error
INFO: creating /opt/ltp/results directory
Checking for required user/group ids
'nobody' user id and group found.
'bin' user id and group found.
'daemon' user id and group found.
Users group found.
Sys group found.
Required users/groups exist.
If some fields are empty or look unusual you may have an old version.
Compare to the current minimal requirements in Documentation/Changes.
ID="arago"
NAME="Arago"
VERSION="2016.12"
VERSION_ID="2016.12"
PRETTY_NAME="Arago 2016.12"
Linux am57xx-evm 4.4.41-rt50-g968d071ce9 #7 SMP PREEMPT RT Mon Jun 3 13:35:30 CST 2019 armv7l GNU/Linux
Gnu C gcc (Linaro GCC 5.3-2016.02) 5.3.1 20160113
Gnu make 4.1
util-linux linux 2.27.1
mount linux 2.27.1 (libmount 2.27.0: assert, debug)
modutils 22
e2fsprogs 1.43-WIP
Linux C++ Library /../lib/libstdc++
Procps 3.3.11
iproute2 iproute2-ss160111
Kbd 2.0.3
Sh-utils --v
Modules Loaded rtc_x1226 bridge stp llc bc_example omap_wdt cbc drbg xfrm_user xfrm4_tunnel ipcomp xfrm_ipcomp esp4 bluetooth ah4 af_key xfrm_algo xhci_plat_hcd xhci_hcd usbcore rpmsg_pru rpmsg_proto rpmsg_rpc dwc3 udc_core pru_rproc pruss_intc ecb virtio_rpmsg_bus snd_soc_simple_card sha512_generic sha512_arm sha256_generic snd_soc_omap_hdmi_audio hmac md5 sha1_generic pvrsrvkm sha1_arm_neon omap_aes_driver sha1_arm pruss omap_sham ahci_platform libahci_platform libahci libata scsi_mod ti_vpe ti_sc ti_csc ti_vpdma dwc3_omap rtc_omap extcon_palmas extcon rtc_palmas snd_soc_tlv320aic3x omap_des omap_rng rng_core omap_remoteproc remoteproc debugss_kmodule virtio virtio_ring sch_fq_codel uio_module_drv uio gdbserverproxy cryptodev cmemk
free reports:
total used free shared buff/cache available
Mem: 1868596 96324 1555172 25176 217100 1718368
Swap: 0 0 0
/proc/cpuinfo
processor : 0
model name : ARMv7 Processor rev 2 (v7l)
BogoMIPS : 12.29
Features : half thumb fastmult vfp edsp neon vfpv3 tls vfpv4 idiva idivt vfpd32 lpae evtstrm
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x2
CPU part : 0xc0f
CPU revision : 2
processor : 1
model name : ARMv7 Processor rev 2 (v7l)
BogoMIPS : 12.29
Features : half thumb fastmult vfp edsp neon vfpv3 tls vfpv4 idiva idivt vfpd32 lpae evtstrm
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x2
CPU part : 0xc0f
CPU revision : 2
Hardware : Generic DRA74X (Flattened Device Tree)
Revision : 0000
Serial : 0000000000000000
no big block device was specified on commandline.
Tests which require a big block device are disabled.
You can specify it with option -z
COMMAND: /opt/ltp/bin/ltp-pan -e -S -a 2264 -n 2264 -p -f /tmp/ltp-XXXXfTiYVJ/alltests -l /tmp/tmp.XZh0MJ -C /opt/ltp/output/LTP_RUN_ON-tmp.XZh0MJ.failed -T /opt/ltp/output/LTP_RUN_ON-tmp.XZh0MJ.tconf
LOG File: /tmp/tmp.XZh0MJ
FAILED COMMAND File: /opt/ltp/output/LTP_RUN_ON-tmp.XZh0MJ.failed
TCONF COMMAND File: /opt/ltp/output/LTP_RUN_ON-tmp.XZh0MJ.tconf
Running tests.......
INFO: ltp-pan reported all tests PASS
LTP Version: 20160510
###############################################################"
Done executing testcases."
LTP Version: 20160510
Result log is in the /tmp/tmp.XZh0MJ "
###############################################################"
Test Start Time: Wed Jun 19 00:36:03 2019
-----------------------------------------
Testcase Result Exit Value
-------- ------ ----------