Tool/software: Linux
Hi,
I have interfaced 3g quectal UC 20 with USB1 port of the Ti 3358 evm board.
I could get up the /dev/ttyUSB interfaces up.
I copied pppd,chat binariesand scripts required for ppp connection ,but when trying to create ppp connection i get following error
root@am335x-evm:~# /usr/sbin/pppd Script /etc/ppp/net-connect finished (pid 995), status = 0x0 Serial connection established. using channel 2 Using interface ppp0 Connect: ppp0 <--> /dev/ttyUSB3 sent [LCP ConfReq id=0x1 <asyncmap 0x0> <magic 0x453e8e8> <pcomp> <accomp>] sent [LCP ConfReq id=0x1 <asyncmap 0x0> <magic 0x453e8e8> <pcomp> <accomp>] sent [LCP ConfReq id=0x1 <asyncmap 0x0> <magic 0x453e8e8> <pcomp> <accomp>] sent [LCP ConfReq id=0x1 <asyncmap 0x0> <magic 0x453e8e8> <pcomp> <accomp>] sent [LCP ConfReq id=0x1 <asyncmap 0x0> <magic 0x453e8e8> <pcomp> <accomp>] sent [LCP ConfReq id=0x1 <asyncmap 0x0> <magic 0x453e8e8> <pcomp> <accomp>] sent [LCP ConfReq id=0x1 <asyncmap 0x0> <magic 0x453e8e8> <pcomp> <accomp>] sent [LCP ConfReq id=0x1 <asyncmap 0x0> <magic 0x453e8e8> <pcomp> <accomp>] sent [LCP ConfReq id=0x1 <asyncmap 0x0> <magic 0x453e8e8> <pcomp> <accomp>] sent [LCP ConfReq id=0x1 <asyncmap 0x0> <magic 0x453e8e8> <pcomp> <accomp>] LCP: timeout sending Config-Requests Connection terminated. Modem hangup
I am using tisdk-rootfs-image-am335x-evm.tar.xz filesystem from am335x-evm-linux-sdk-bin-05.03.00.07.tar.xz
Please let me know how to add the ppp support in the root file system and build the root filesystem.