This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

problem with: booting via TFTP Using NFS File System



I have a problem with booting via TFTP

printenv tells me that tftpserverip ist set to 150.100.7.240, witch is the ip of my host running ubuntu with NFS and TFTP server on it:

DM355 EVM # printenv                                                           
bootdelay=3                                                                    
baudrate=115200                                                                
filesize=248448                                                                
fileaddr=82000000                                                              
ipaddr=150.100.7.137                                                           
nboot0x80700000=0 0x400000;bootm                                               
nfshost=150.100.7.132                                                          
nfshost=150.100.7.240                                                          
rootpath=/home/praktikant/workdir/filesys                                      
serverip=150.100.7.240                                                         
stdin=serial                                                                   
stdout=serial                                                                  
stderr=serial                                                                  
videostd=pal                                                                   
bootcmd=dhcp;bootm                                                             
bootargs=console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=150.1l
bootfile=uImage                                                                
                                                                               
Environment size: 608/16380 bytes             

 

but when I use the boot command, my evm is trying to boot from another IP address

                                 
DM355 EVM # boot                                                               
BOOTP broadcast 1                                                              
DHCP client bound to address 150.100.7.137                                     
TFTP from server 150.100.7.3; our IP address is 150.100.7.137                  
Filename 'uImage'.                                                             
Load address: 0x80700000                                                       
Loading: T T