This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5718: 12-bit grayscale VIP input

Guru 16800 points
Part Number: AM5718

Tool/software: Linux

Hello,

We have several questions about VIP on AM5718.

1.Could you tell me whether AM5718 running PROCESSOR-SDK-LINUX-RT-AM57X (v5.2) support 12-bit RAW data input into VIP?
  At page 1893 in TRM, "24-bit data input plus discrete syncs can be configured to include: 12/16-bit RAW Capture" is described.
  However, VIP Driver doesn't support 16-bit RAW capture (I think this includes 12-bit RAW data capture), which is described in the following URL.
  software-dl.ti.com/.../Foundational_Components_Kernel_Drivers.html

2.Can we use the 16-bit wide in the UYVY mode as a 12-bit RAW data input port?
  We want to know whether we can capture 12-bit RAW data in the UYVY mode.

Best Regards,
Nomo