This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

rt73 wifi driver for IPNC based on DM355



Hello everyone:

I followed this wiki to try to use the wifi on the IPNC based on DM355.

http://tiexpressdsp.com/wiki/index.php?title=Wireless_USB_Network

But I only have a TP-LINK USB Wifi adapter based on RT2571W/rt73 chipset.

so I launched kernel config and enabled the RADIO support and the USB-host support.

And because the mini-USB port on the IPNC is have not any power supply, I added a 5V DC on it.

And I download the 2009_0206_RT73_Linux_STA_Drv1.1.0.2 on Ralink, Compiled it, and got the rt73.ko successfully.

then:

# insmod rt73.ko    
usbcore: registered new driver rt73

But, when I used the command "ifconfig rausb0 up",the IPNC printed:

# ifconfig rausb0 up
modprobe: FATAL: Could not load /lib/modules/2.6.10_mvl401_IPNC-2.1.0/modules.dep: No such file or directory

SIOCGIFFLAGS: No such device

modprobe: FATAL: Could not load /lib/modules/2.6.10_mvl401_IPNC-2.1.0/modules.dep: No such file or directory

SIOCGIFFLAGS: No such device

or use "ifconfig -a":

# ifconfig -a
eth0      Link encap:Ethernet  HWaddr 00:00:00:00:00:00  
          inet addr:192.168.1.101  Bcast:192.168.255.255  Mask:255.255.0.0
          inet6 addr: fe80::200:ff:fe00:0/64 Scope:Link
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:11204 errors:0 dropped:0 overruns:0 frame:0
          TX packets:6475 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:3730129 (3.5 MiB)  TX bytes:1009686 (986.0 KiB)
          Interrupt:53 Base address:0x2000

lo        Link encap:Local Loopback  
          inet addr:127.0.0.1  Mask:255.0.0.0
          inet6 addr: ::1/128 Scope:Host
          UP LOOPBACK RUNNING  MTU:16436  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:0
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

sit0      Link encap:UNSPEC  HWaddr 00-00-00-00-31-00-00-00-00-00-00-00-00-00-00-00  
          NOARP  MTU:1480  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:0
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

 

I have no idea how to resolve it, who can help me??

Thanks.