Part Number: TDA2SX
Tool/software: Linux
Hi all,
I am working on TI EVM TDA2x board with cpu as "DRA752-GP ES2.0" & DRAM = 4GB
In the below link some discussions happened on DDR3 size and memory configuration,So with out "mem" argument in uenv.txt we can use our total available RAM set up on our Board.
http://e2e.ti.com/support/processors/f/791/p/803805/3006811#3006811
I tested with, without mem argument in uenv.txt and it is fine it is displaying total mapped memory.
root@dra7xx-evm:~# cat /proc/meminfo
MemTotal: 3717752 kB
MemFree: 3594484 kB
MemAvailable: 3648292 kB
But here,my problem is if i'm going to limit memory to 2GB with mem argument(mem=2048M) then kernel panic happened.I don't know why it happened.See the below log.
[ 2.804088] Freeing unused kernel memory: 340K
[ 2.808566] This architecture does not have kernel memory protection.
[ 2.826244] Unhandled fault: synchronous external abort (0x210) at 0xffeee000
[ 2.833411] pgd = c0003000
[ 2.836128] [ffeee000] *pgd=80000080007003, *pmd=affa6003, *pte=c00000ffc0071f
[ 2.843413] Internal error: : 210 [#1] PREEMPT SMP ARM
[ 2.848570] Modules linked in:
[ 2.851646] CPU: 1 PID: 1 Comm: swapper/0 Not tainted 4.4.84-00027-g018eb62-dirty #147
[ 2.859595] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 2.865716] task: ee878000 ti: ee862000 task.ti: ee862000
[ 2.871142] PC is at memcpy+0x48/0x330
[ 2.874914] LR is at copy_to_iter+0x194/0x2ac
[ 2.879290] pc : [<c02b0ca8>] lr : [<c02c3750>] psr: 60000013
[ 2.879290] sp : ee863d0c ip : 00000000 fp : ee863d5c
[ 2.890816] r10: 00000000 r9 : ffeee080 r8 : ee863e2c
[ 2.896061] r7 : 00000080 r6 : ee863e34 r5 : 00000080 r4 : 00000080
[ 2.902614] r3 : 00000002 r2 : 00000000 r1 : ffeee000 r0 : ee308c00
[ 2.909168] Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
[ 2.916507] Control: 30c5387d Table: 80003000 DAC: 55555555
[ 2.922277] Process swapper/0 (pid: 1, stack limit = 0xee862210)
[ 2.928309] Stack: (0xee863d0c to 0xee864000)
[ 2.932682] 3d00: 00000080 ee863e34 00000080 ee863e2c ee308c00
[ 2.940895] 3d20: 00000080 c02c3750 eed933f4 ee863d74 ee863d64 00001000 ee863e34 ffeee000
[ 2.949107] 3d40: 00000000 ee5835b0 ee862000 00000000 ee863d9c ee863d60 c02c39bc c02c35c8
[ 2.957321] 3d60: c00d0010 c067ee50 eff91000 eff91000 00000000 eff91000 ee583694 edc07780
[ 2.965534] 3d80: 00000000 ee5835b0 ee862000 00001000 ee863e1c ee863da0 c00d19dc c02c3874
[ 2.973747] 3da0: 00000001 ee3d2400 00000000 c093266c 00080001 00000000 ffffffff 00000001
[ 2.981959] 3dc0: edc077e8 00000fff 00000000 ffffe000 ee863e48 ee863e34 c01cb134 c01c530c
[ 2.990169] 3de0: 00000014 00000014 ee863e24 ee863df8 c0143af4 edc07780 ee863ec0 00000000
[ 2.998384] 3e00: 00000000 00000080 00000000 edc0e000 ee863e8c ee863e20 c01207b4 c00d1778
[ 3.006596] 3e20: 00000080 c0143aac c0111554 ee308c00 00000080 00000002 00000000 00000080
[ 3.014809] 3e40: ee863e2c 00000001 edc07780 00000000 00000000 00000000 00000000 00000000
[ 3.023022] 3e60: 00000000 00000000 ee308c00 edc07780 ee863ec0 c0935668 ee308c00 ee3f5000
[ 3.031234] 3e80: ee863ebc ee863e90 c0120f58 c012070c 0000003f 00000000 ffffe000 00000000
[ 3.039446] 3ea0: c09355e0 c0935668 ee308c00 ee3f5000 ee863edc ee863ec0 c01262ac c0120ee4
[ 3.047658] 3ec0: 00000000 00000000 ee308c00 ee5835b0 ee863f04 ee863ee0 c0126e18 c0126278
[ 3.055870] 3ee0: ee308c00 00000080 00000003 ee1ba000 c09355e0 c0935668 ee863f4c ee863f08
[ 3.064082] 3f00: c01276fc c0126d64 c0982e58 00000000 ffffe000 00000000 00000000 00000000
[ 3.072294] 3f20: c09355e0 c09355e0 c0935668 00000000 00000000 00000000 00000000 00000000
[ 3.080503] 3f40: ee863f64 ee863f50 c01278cc c0127280 00000000 00000000 ee863f7c ee863f68
[ 3.088715] 3f60: c000974c c01278ac c0982000 c0813728 ee863f94 ee863f80 c0009764 c000972c
[ 3.096928] 3f80: c0982000 c067d630 ee863fac ee863f98 c067d6d4 c000975c 00000000 c067d630
[ 3.105143] 3fa0: 00000000 ee863fb0 c000fb88 c067d63c 00000000 00000000 00000000 00000000
[ 3.113355] 3fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 3.121567] 3fe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000000
[ 3.129778] Backtrace:
[ 3.132244] [<c02c35bc>] (copy_to_iter) from [<c02c39bc>] (copy_page_to_iter+0x154/0x2c0)
[ 3.140453] r10:00000000 r9:ee862000 r8:ee5835b0 r7:00000000 r6:ffeee000 r5:ee863e34
[ 3.148354] r4:00001000
[ 3.150909] [<c02c3868>] (copy_page_to_iter) from [<c00d19dc>] (generic_file_read_iter+0x270/0x67c)
[ 3.159989] r10:00001000 r9:ee862000 r8:ee5835b0 r7:00000000 r6:edc07780 r5:ee583694
[ 3.167891] r4:eff91000
[ 3.170449] [<c00d176c>] (generic_file_read_iter) from [<c01207b4>] (__vfs_read+0xb4/0xdc)
[ 3.178744] r10:edc0e000 r9:00000000 r8:00000080 r7:00000000 r6:00000000 r5:ee863ec0
[ 3.186642] r4:edc07780
[ 3.189195] [<c0120700>] (__vfs_read) from [<c0120f58>] (vfs_read+0x80/0x10c)
[ 3.196357] r9:ee3f5000 r8:ee308c00 r7:c0935668 r6:ee863ec0 r5:edc07780 r4:ee308c00
[ 3.204179] [<c0120ed8>] (vfs_read) from [<c01262ac>] (kernel_read+0x40/0x54)
[ 3.211341] r9:ee3f5000 r8:ee308c00 r7:c0935668 r6:c09355e0 r5:00000000 r4:ffffe000
[ 3.219165] [<c012626c>] (kernel_read) from [<c0126e18>] (prepare_binprm+0xc0/0x120)
[ 3.226936] r5:ee5835b0 r4:ee308c00
[ 3.230541] [<c0126d58>] (prepare_binprm) from [<c01276fc>] (do_execveat_common+0x488/0x62c)
[ 3.239010] r7:c0935668 r6:c09355e0 r5:ee1ba000 r4:00000003
[ 3.244727] [<c0127274>] (do_execveat_common) from [<c01278cc>] (do_execve+0x2c/0x34)
[ 3.252587] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0935668
[ 3.260484] r4:c09355e0
[ 3.263041] [<c01278a0>] (do_execve) from [<c000974c>] (run_init_process+0x2c/0x30)
[ 3.270732] [<c0009720>] (run_init_process) from [<c0009764>] (try_to_run_init_process+0x14/0x44)
[ 3.279637] r5:c0813728 r4:c0982000
[ 3.283246] [<c0009750>] (try_to_run_init_process) from [<c067d6d4>] (kernel_init+0xa4/0xf4)
[ 3.291716] r5:c067d630 r4:c0982000
[ 3.295326] [<c067d630>] (kernel_init) from [<c000fb88>] (ret_from_fork+0x14/0x2c)
[ 3.302924] r5:c067d630 r4:00000000
[ 3.306531] Code: ba000002 f5d1f03c f5d1f05c f5d1f07c (e8b151f8)
[ 3.312651] ---[ end trace 77b1d46e3a24be20 ]---
[ 3.317287] note: swapper/0[1] exited with preempt_count 1
[ 3.323144] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
[ 3.323144]
[ 3.332323] CPU0: stopping
[ 3.335048] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G D 4.4.84-00027-g018eb62-dirty #147
[ 3.344216] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 3.350332] Backtrace:
[ 3.352806] [<c00131d4>] (dump_backtrace) from [<c00133d0>] (show_stack+0x18/0x1c)
[ 3.360405] r7:c0931ef0 r6:20000193 r5:00000000 r4:c094f810
[ 3.366128] [<c00133b8>] (show_stack) from [<c02b21a8>] (dump_stack+0x8c/0xa0)
[ 3.373386] [<c02b211c>] (dump_stack) from [<c0016520>] (handle_IPI+0x184/0x198)
[ 3.380811] r7:c0931ef0 r6:00000000 r5:00000000 r4:c092c424
[ 3.386530] [<c001639c>] (handle_IPI) from [<c00094c4>] (gic_handle_irq+0x78/0x7c)
[ 3.394127] r7:fa212000 r6:c0931ef0 r5:fa21200c r4:c09328ec
[ 3.399846] [<c000944c>] (gic_handle_irq) from [<c0013ec0>] (__irq_svc+0x40/0x74)
[ 3.407357] Exception stack(0xc0931ef0 to 0xc0931f38)
[ 3.412428] 1ee0: 00000001 00000000 fe600000 00000000
[ 3.420641] 1f00: c0930000 c09324ac 00000000 00000000 c0931f60 c0686284 c093250c c0931f4c
[ 3.428850] 1f20: c0931f2c c0931f40 c0027fec c0010600 60000013 ffffffff
[ 3.435487] r9:c0686284 r8:c0931f60 r7:c0931f24 r6:ffffffff r5:60000013 r4:c0010600
[ 3.443314] [<c00105d8>] (arch_cpu_idle) from [<c0071468>] (default_idle_call+0x28/0x34)
[ 3.451442] [<c0071440>] (default_idle_call) from [<c00716c8>] (cpu_startup_entry+0x200/0x260)
[ 3.460095] [<c00714c8>] (cpu_startup_entry) from [<c067d62c>] (rest_init+0x90/0x94)
[ 3.467868] r7:00000000
[ 3.470426] [<c067d59c>] (rest_init) from [<c08dbd88>] (start_kernel+0x400/0x40c)
[ 3.477936] r5:c0982000 r4:c0982040
[ 3.481543] [<c08db988>] (start_kernel) from [<80008090>] (0x80008090)
[ 3.488103] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
[ 3.488103]
If I'm putting mem=1024M or mem=1536M then the board is booting fine and displaying the memory info as follows.
root@dra7xx-evm:~# cat /proc/meminfo(for 1GB or mem=1024M)
MemTotal: 615952 kB
MemFree: 496928 kB
MemAvailable: 573456 kB
root@dra7xx-evm:~# cat /proc/meminfo(for 1.5G or mem=1536M)
MemTotal: 1135628 kB
MemFree: 1013800 kB
MemAvailable: 1085724 kB
Buffers: 8204 kB
Could you please help me to solve the issue. Is there any thing I need to modify/I need enable any configuration in u-boot & kernel.Please tell me.
Thanks & Regards,
A.Kavya Harini
root@dra7xx-evm:~# cat /proc/meminfo
MemTotal: 615952 kB
MemFree: 496928 kB
MemAvailable: 573456 kB