This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C62x/C64x Fast Run-Time Support (RTS) Library Release notes

Hi Team,

Our customer is requesting for the release notes of the C62x/C64x Fast RTS Library.

The Programmer's Reference stated that the spru653.pdf document in the root directory of every release contains the updates, but these documents seems to be exactly the same for each version.

Do we have an explicit reference or page which contains their respective version updates?

Thank you so much in advance for your help.


Regards,

Jejomar

  • Hi,

    Do we have an explicit reference or page which contains their respective version updates?

    Not that I know of. Let me check with the design team, feedback will be posted directly here.

    Best Regards,
    Yordan

  • Hi Yordan,

    Thank you so much for your response. We'll be waiting for the update.


    Kind Regards,

    Jejomar

  • Jejomar,

    The release for fastRTS C62x/C64x platforms was done in 2012 and the update were minor to enable support for ELF binaries (C6000 compiler 8.x only supports ELF binaries) and bug fixes to inlined functions as indicated in the readme62x64x in the folder fastRTS_c62xc64x_1_42\c6400\mthlib

    As per the ReadMe the following updates were made:

    ---------------------------------------------------------------------------------
    Updates
    ---------------------------------------------------------------------------------
    * ELF version of the library
    * Bug fix for addsp_i and subsp_i functions

    I have checked SDOCM and there are no known issues for the library as far as I can tell. If this is an existing design using then we recommend using C6000 compiler 7.x or 6.x as latest 8.x compiler has stopped support for COFF binaries.

    Regards,

    Rahul