This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can not fild DM365 DVEVM Software



Dear everyone!

  I've just got the DM365 DVEVM, and then follow the instruction of "GSG: DM365 DVEVM Software Setup" to setup software platform on linux, but i can not find the following Software packages: 

1. mvl_5_0_demo_target_setuplinux.bin

2. mvltools5.0-no-target.tar.gz

3. DaVinciLSP_#_#_#_#.tar.gz

anybody who can tell me where to find those packages? Thanks!

  • Sorry for the confusion on these.

    tony lee said:
    1. mvl_5_0_demo_target_setuplinux.bin

    This file no longer exists, and I have edited the wiki page to reflect that, the contents that would have been in this file are now in the mvl_5_x_x_demo_sys_setuplinux.bin so you just have to install one instead of two binaries.

    tony lee said:

    2. mvltools5.0-no-target.tar.gz

    3. DaVinciLSP_#_#_#_#.tar.gz

    These two files are generated by running the binaries, the mvltools comes from the ...sys_setuplinux.bin and the DaVinciLSP comes from the ...lsp_setuplinux_x_x_x_x.bin. The installer is really just a way of accepting a license agreement, the actual install content are just these gzip files.

  • Dear Bernie, thanks for your rapid reply, i will follow you instruction and try again.
  • Dear Bernie,

    I met a different issue.

    After installing ./mvl_5_x_x_demo_sys_setuplinux.bin file I jsut got one file in my /opt/mv_pro_5.0 folder as:

    1. mvltools5_0801921_update.tar.gz

    Waiting for your valuable reply.

    Thank you.

    Regards,

    Prashant