hi ,
I have several question about dm355 multi-stream.
First, in my dm355 platform, there are 4 stream with 2 resolution can be work well at the same time such as : 720*480 MPEG4, 352*240 MPEG4, 720*480 MotionJPEG, 352*240 MotionJPEG. If I change resolution to 640*480 or 160*112, the video will be unnormally and it looks like this->. 
But 352*240 is OK. I checked all resolution setting(capture.c, writer.c, video.c in encode stream) in every step was correct. Maybe I lost some key point about this question. Have anyone can give me some hints to correct this error?
Second, in Peripheral Reference Guide for DM350 Subsystem VPFE , chapter "Horizontal & Vertical Resize Module",
"The sizes of output images are limited to below 1344 pixels/line for RSZ[0] and 640 pixels/line for RSZ[1]."
Is everyone can give me some reference or concept about RSZ? ex: Surrpose that i have "4" stream at the same time, what is the actually progress in "2" resizers? How can i programable control it?
ps: My English is very poor. Thanks a lot for your patiences to understand my article.
Have a nice day.