Part Number: AM3352
I want to know if we can make the two built-in Ethernet ports into separate, non-switched ports?
Also, if the two ports act as a switch do they support RSTP?
Thanks
Viktorija
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM3352
I want to know if we can make the two built-in Ethernet ports into separate, non-switched ports?
Also, if the two ports act as a switch do they support RSTP?
Thanks
Viktorija
Viktorija Cecil said:I want to know if we can make the two built-in Ethernet ports into separate, non-switched ports?
Yes, this is called Dual EMAC mode.
Viktorija Cecil said:Also, if the two ports act as a switch do they support RSTP?
I have asked the CPSW experts to comment. They will post here.
DK, follow up question:
I thought there was an issue with the dual EMAC mode where it was using VLAN tags to distinguish between the two ports. Not all devices can support these VLAN tags. Is there a way to filter the VLAN tags before they leave the CPU?
Hi,
That is correct that not all devices can support VLAN tagging and the packets are filtered as you suggest. The rules loaded into the ALE that setup the VLANs to emulate the dual mac configuration are defined so the VLAN tag is stripped on packet egress.
Best Regards,
Schuyler