This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TMDSICE3359: HSR/PRP debug error

Part Number: TMDSICE3359


Tool/software: TI-RTOS

Hello,

I've the TMDSICE3359 and I want to implement HSR protocol on it.

To do that, I've download :

- PRU ICSS SW for HSR/PRP v01.00.04.02

- Processor SDK TI RTOS v4.03.00.05

- CCS 7.4.0.00015

I have also target my board and import the HSR project (that I've find in the PRU ICSS SW for HSR/PRP).

But after running that the project stop and it is written "Suspend - SW breakpoint" like you can see in the PDF.

Can you please explain me what I 've to do now to implement the hsr_app provides in the PRU ICSS SW for HSR/PRP? thanks for your helpSuspend SW breakpoint.pdf