This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM65X: Arago build hangs

Part Number: PROCESSOR-SDK-AM65X

Tool/software: Linux

Hi ,

I was trying to build minimal file system image for am65xx.

Currently  2 running tasks (2492 of 4788)  52% |################################################                                              |
0: external-linaro-toolchain-2017.11-r0.arago36 do_fetch (pid 11253)  40% |#####################                                 | 496.00 KiB/s
1: pcitest-4.9-r0 do_fetch - 12512s (pid 20362)

It is got stuck on this point for a while. I checked with my network everything is fine.

Can you help me on this.

Thanks and Regards,

Vishnu