Part Number: OMAP-L138
Hi E2E,
Good day!
What is the maximum storage density that can be used on the SATA and MMC interfaces?
Thank you for your usual support.
Best regards,
Franz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OMAP-L138
Hi E2E,
Good day!
What is the maximum storage density that can be used on the SATA and MMC interfaces?
Thank you for your usual support.
Best regards,
Franz
Hi Franz,
The OMAP-L138 device includes an two MMCSD controllers which are compliant with MMC v4.0, Secure Digital Part 1 Physical Layer Specification V1.1 and Secure Digital Input Output (SDIO) V2.0 specifications. Which means you can use SD cards with max size up to 32 GB.
The SATA Controller supports AHCI controller spec 1.1 and 1.5 Gbps (Gen1i) and 3 Gbps (Gen2i) line speeds. The limitation comes from 32-bit addressing space but 64-bit addressing space is not supported. If the block size is 512 bytes the limitation is 2 TB (512 * 2 ^ 32 bytes). Of course the limitation can be caused by used file system.
You can find more details about OMAP-L1x Serial ATA at:

Regards,
Tsvetolin Shulev
Hi Franz,
Regarding MMC, I think that any sd card compliant with the standards described in Section 27.1.5 Industry Standard(s) Compliance Statement of the TRM should work with OMAP-L138 devices. I have not heard of tested maximum supported storage density.
Same thing applies for SATA, the storage device should comply with Section 29.1.2 Features Supported and you should also have in mind Section 29.1.3 Features Not Supported.
Best Regards,
Yordan
One more thing to point out along with all the helpful guidance Yordan has provided, especially if this is a new design.
It would be good for you/your customer to be aware of the Silicon advisory 2.3.22 on SATA for these devices
http://www.ti.com/lit/er/sprz301m/sprz301m.pdf
This has unfortunately been a show stopper for several customers who want to use SATA on this device, given most HDDs are now GEN3 etc.
Regards
Mukul
Hello,
Thanks to all of you. This is very helpful. Will inform my customer regarding this.
Best regards,
Franz