Hi All,
I have an DM365 application which was working fine with the DVSDK 2_10_00_08. I tried to upgrade to the newer 2_10_00_14 but I got some errors.
1. I found that the framework components directory in the erstwhile 2_10_00_08 was framework_components_2_23_00_03; whilst the one in the newer SDK is framework_components_2_23_00_02. Is this correct or do I seem to have some wrong installations?
2. I get the error "ti.sdo.fc.rman" along the path when I use the framework_components_2_23_00_02; but it does not give any errors when I use the framework_components_2_23_00_03.
3. After a successful build with the framework_components_2_23_00_03 component + application + DVSDK 2_10_00_14, my application crashes saying that
++++++
EDMA Error: init: major version mismatch between interface and driver.
EDMA Error: needs driver version 0x1100000, got 0x1000000
Encode Error: Failed to open video encode algorithm: h264enc (0x0)