This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Flashing UBoot and UBL

Hi,

I need to flash UBoot and UBL into the brand new NAND chip (MT29F16G08DAA).  I have tried flashing with the serial utility and it says that everything is written correctly, but when I cycle the power, and turn on a serial application, nothing shows up, so I do not think things are working as they should be.  Also I tried to connect through Segger JLink through the ARM JTAG 20 pin connector on DM355 EVM, but doesnt seem to recognize the board.

What am I doing wrong?