This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2E: TDA4 simulation ti_cnnperfsim.out

Part Number: TDA2E

hi  i have TDA4 sdk packege. ti_cnnperfsim.out which is display ti cycle be included . it run ok by sample(jacintoNet11v2.cfg) but I can't to find input image data. Does he generate his own image data internally?

  • Hi,

    What is the software package you are referring to?

    Regards,

    Rishabh

  • thanks for your reply.

     I get the package(TIDL4J7.zip).

     

  • thanks for your reply.

     I get the package(TIDL4J7.zip ). tidl_j7_00_05_00_00

    I run PC_dsp_test_dl_algo.out.exe ,it need input image data by the option(inData) of Inference Configuration Parameters.

    like this

    inData Input tensors File for Reading

    But I can’t find parameter to set input Image data in configure parameters. Is it no need input image data?

    configuration file:

    NUMCORES = 1
    #DDR_EFFICIENCY parameter is external to SOC, Practically 60% efficiency is achieved in real system,
    #but be careful while comparing with other benchmarks and make sure that it is conisdered in other benchmarks similarly
    DDR_EFFICIENCY = 0.6
    NUMEMIF_PORTS = 1
    #0: 8-bit, 1: 16-bit
    DATATYPE = 0
    FILENAME_NET = "../../test/testvecs/models/public/caffe/jacintoNet11v2/deploy.prototxt"
    FILENAME_PARAMS = "../../test/testvecs/models/public/caffe/jacintoNet11v2/imagenet_jacintonet11v2_iter_320000.caffemodel"
    #0: caffee, 1: TensorFlow
    FILEFORMAT_NET = 0
    OUTPUT_DIR = jacintoNet11v2
    #optional
    INWIDTH = 1024
    INHEIGHT = 512
    NUMCHANNELS = 3
  • Hi,

    Please get in touch with your TI representative for any information related to this package.

    Regards,

    Rishabh