Part Number: TMS320C5535
Hello,
we are developing an intercom unit which uses aer/aec algorithms. Regarding gain calibration, we don't have to meet standard specifications. So we start with a nominal value for adc, dac and output amplifier gains.
Questions:
1. Parameter gain_rx_analog in aerControl_s struct:
Do we have to set this parameter to the same value as the dac + output amplifier gain? So if we start with nominal dac + output amplifier gain of 20dB, should we set this parameter to 20*16=320? When speaker volume is changed, should we adapt this parameter?
2. Same question as 1. for gain_tx_analog and pga gain
3. We use aic3254 codec and have agc activated. So in aer/aec we don't use agc block. Is this allowed?
Thanks in advance
Marc